2011-11-25 10:31 AM
Any one with ideas on this one, I`ve never seen this on other micros:
STM32F103RE6 I have a simple application, an asyc pulse stream of data bits: 2.4mS and 1.2mS MAX 2.4mS = 1, 1.2mS = 0 Unfortunately the design does not allow for CCP, So I have to sample on both edges an keep count.... NVIC_InitStructure.NVIC_IRQChannel = EXTI9_5_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); I have tried all combinations of priorities etc... I try to sample on BOTH edges and lo and behold the micro misses the edges, I have DISABLED ALL other interrupts, stopped all other processes and ONLY have the Interrupt running, I have a simple ''follow the leader'' pin that pulses high every time the interrupt happens and clears everytime the interrup exits. void EXTI9_5_IRQHandler(void) { EXTI->PR = EXTI_LINE_RFRX; BL_ON; //make pin high here !! Reset the pin in MAIN while loop } The ''follow the leader'' pin GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init( GPIOC, &GPIO_InitStructure ); The input pin where the INTERRUPTS are sampled GPIO_InitStructure.GPIO_Pin = GPIO_PIN_RFRX; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU; GPIO_Init(GPIOC, &GPIO_InitStructure); /* PCLK1 = HCLK/2 */ RCC_PCLK1Config(RCC_HCLK_Div2); This is running at 1/2 HCLK, but even when I set it to HCLK, NO DIFFERENCE edges are still missed. I also tried the other route 1 edge at a time falling or rising samples are missed on a regular bases ?? it seems maninly the falling edges...2011-11-26 1:04 PM
The obvious concern here is that you're relying on main() to clear your pin - if a couple of interrupts come in quick succession then main() might not get a chance, making you believe you missed one of the interrupts (you'd probably think you missed the second one). First thing I would try is setting and clearing your pin in the IRQ handler. Something like this:
void EXTI9_5_IRQHandler(void) { EXTI->PR = EXTI_LINE_RFRX; BL_ON; //make pin high here !! Reset the pin in MAIN while loop BL_OFF; } Then it becomes a simple matter to setup your scope to trigger off the interrupt source, with this pin as a second trace, and you'd be able to see if indeed you miss any.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.