2018-10-31 11:35 PM
Hi,
What is the minimum latch time for BOOT0 pin (after reset) in order to get the MCU to internal ST bootloader mode? Is there timing diagram somewhere?
FYI, I am using STM32L475 MCU.
Thank you,
Yuval
2018-11-06 2:44 AM
Hello,
On STM32L475, the Boot0 pin is latched on the rising edge of the NRST pin.
We do not specify an hold time required on this Boot0 pin versus the NRST pin.
Even if the Boot0 pin switches from 1 to 0 immediately after reset release, the MCU will enter bootloader mode.
Kind Regards,
Imen
2018-11-06 3:00 AM
It is 4 SYSCLK after reset
2018-11-06 4:13 AM
Any source? Link?
JW
2018-11-06 2:38 PM
Thank you for your answer.
Let me just make sure I understand, once NRST goes high, Boot0 latch time should only be > 0. Is my understanding correct?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.