2008-11-18 11:08 AM
migration from uPSD3200 to STM32
2011-05-17 3:50 AM
2011-05-17 3:50 AM
Cortex code size is about 1/4 the size of 8051 code according to
www.iqmagazineonline.com/IQ/IQ16/LowRes.pdfs/Luminary(pg28-32)IQ16.pdf2011-05-17 3:50 AM
Quote:
On 04-11-2008 at 04:55, Anonymous wrote: Cortex code size is about 1/4 the size of 8051 code according tohttp://www.iqmagazineonline.com/IQ/IQ16/LowRes.pdfs/Luminary(pg28-32)IQ16.pdf
All that article actually says is,Quote:
... ARM reports that Cortex-M3 requires about 1/4th the code space of an 8051.
No reference is given to how ARM arrived at that figure, how generally applicable it is, etc, etc - and, of course, ARM's is hardly an independent view in this matter, is it...?! ;) The context in the article is,Quote:
... an 8-bit CISC machine like the 8051 is actually a very inefficient architecture for modern high-level software.
Which is assuming that the 8051 is being used inappropriately - so, if you have a well-optimised, appropriate 8051 application, I guess the comparison will be very different...? So, does anyone have a reference to the original ARM publication that made this ''25%'' claim? [ This message was edited by: st7 on 11-11-2008 18:12 ] [ This message was edited by: st7 on 11-11-2008 18:13 ]2011-05-17 3:50 AM
Quote:
if you have a well-optimised, appropriate 8051 application, I guess the comparison will be very different...?
The Keil documentation seems to provide a more realistic illustration:http://www.keil.com/support/man/docs/gs/gs_ma_portaccess.htm
illustrates a case where the 8051 requires only 25% of the code size of a corresponding Cortex program; Whereashttp://www.keil.com/support/man/docs/gs/gs_ma_pointeraccess.htm
illustrates a case where the Cortes requires 25% of the code size of a corresponding 8051 program! Thus, as I suspected, it depends very much on the specific nature of your particular application - and any so-called ''general'' figures you may see must be taken with great caustion!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.