2022-05-01 5:32 AM
hey there
I have a stm32f103 blue pill board which I wish to generate MHz frequencies on pinC13.
I have used TIM1. it starts and interrupts and on each interrupt I toggle PC13
like so
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if(htim->Instance == TIM1)
{
HAL_GPIO_TogglePin(GPIOC,GPIO_PIN_13);
}
}also I set APB1 to 64MHz in Cube.
and here is my TIM1 config(this part is generated by Cube so I just bring up the Prescaler and Period part )
htim1.Instance = TIM1;
htim1.Init.Prescaler = 0;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = 1;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;as you can see with these Prescaler and Period I should have frequency around 64000000/(0+1)(1+1)~32MHz
but on Oscilloscope I see around 125kHz!
I know my oscilloscope TIM/DEV is limited to us but at least I expect to see to parallel lines showing high frequency
what is the problem?
2022-05-01 5:41 AM
You should use the TIM to drive/toggle pin a directly, without interrupts, if you don't want to saturate the MCU.
Depending on how efficient your interrupt code is, a few hundred KHz is the ceiling.
2022-05-01 5:46 AM
@Community member "You should use the TIM to drive/toggle pick a directly, without interrupts, if you don't want to saturate the MCU."
you mean should I use PWM connected to TIM1?
"Depending on how efficient your interrupt code is, a few hundred KHz is the ceiling."
I guess it is quit efficient, cause I have nothing else in my code...
so how can I generate MHz frequencies on a pin?
2022-05-01 6:16 AM
2022-05-01 7:34 AM
Should have read pin, not pick, darn auto-complete..
The TIM should have PWM and Toggle modes. Doesn't have to be TIM1, pick a TIMx/CHx associated with a pin.
>>I guess it is quite efficient, cause..
You're using HAL, the processor is counting instructions, figure at least 2x the friction there.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.