2024-07-04 4:22 AM
Dear all,
I'm working on a project with a waveshare eink display. I'm using the STM32F103RET6 controller and CubeIDE as development environment. I'm building my application as a c++ application with the FreeRTOS lib.
My Display class has a 4000 byte buffer containing the current image. I initialize the buffer as all 0's and this works fine. However, during the code that prepares the image with some text, the buffer seems to get written from a different place in the application. When I set a watchpoint on one of the bytes in the buffer that gets written, It triggers on the TIM1 IRQ handler. Tim1 is used as sys clock. (see image for the trace) I don't see any relation between this timer and the buffer.
Any idea how to debug this situation? Many thanks in advance!
Regards, JOK
2024-07-04 6:24 AM
> I don't see any relation between this timer and the buffer.
Show context - source, disasm of code before the point where it stops, processor registers.
JW
2024-07-15 11:02 AM
Sorry, this question can be closed. I forgot to add a reference symbol in a function that needs my display object as argument. Instead of the reference it created a copy of the display object and this gave strange behavior.Thanks anyway
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.