2015-09-29 2:52 AM
hi, I'm trying to turn ON and OFF the LEDs of my board with 10-second intervals, but I get results in about 8 seconds.
This is my code, I did not understand the frequencies of the processor card. I apologize, I'm just a student.#include ''stm32f4xx.h''
void sleep(float, int);
//accensione di un led
int main (void){
RCC->AHB1ENR |=0X8; //Enable port D
RCC->APB1ENR |=1; // Enable TIM2 32 bit
GPIOD->MODER |=0x55<<
24
; // Enable LEDs
TIM2->PSC = 0;
TIM2->ARR = 48000000;
TIM2->CR1 |= 1; //Enable timer putting 1 on CEN register
TIM2->CNT = 0; //start counting
while(1){
if((TIM2->SR & 1) != 0){
if((GPIOD->ODR & (1<<
15
)) == 0)
GPIOD->ODR |= 1<<
15
;
sleep(10,1);
if((GPIOD->ODR & (1<<
15
)) != 0)
GPIOD->ODR &= ~(1<<15);
sleep(10,1);
}
}
}
void sleep(float mhz, int sec){
float hz = mhz*1000000;
float t = 1/hz;
int i = 0;
for(i = 0; i < (int)sec/t; i++);
}
#stm32f401
2015-09-29 5:44 AM
Is the processor configured to run at 84 MHz? review the system_stm32f4xx.c file
Values programmed into the Period (ARR) are in the form N-1 The Update status bit in SR needs clearing if you're pacing on that.TIM2->SR = ~1; // not RMW formYour software delay is of some what arbitrary, as it's hard to establish a C line to processor instruction, and the optimizer might establish your loop is pointless and remove it. Consider a volatile iterator.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.