2010-11-04 1:38 AM
Meaning off GPIO_Speed declaration
2011-05-17 5:13 AM
Please see RM0008 Reference manual section 8.1.
Output MODE bits MODE[1:0] Meaning 00 Reserved 01 Max. output speed 10 MHz 10 Max. output speed 2 MHz 11 Max. output speed 50 MHz Also see the Data Sheet for your device and look at the Electrical characteristics / Input/output AC characteristics. Basically, choose lower speed if you don't need fast clocks or edge transitions. It will reduce EMC problems.2011-05-17 5:13 AM
See also SLEW RATE CONTROL
If you drive the pin aggressively to get sharp edges, and over come line capacitance, you will typically see more over-shoot/under-shoot, and ringing, in the output signal.2011-05-17 5:13 AM
Well, he does have a point. Table 19 shows these values for MODE. But no where does RM0008 explain what they mean. The STM32F103ZE (which I use) data sheet table 47 has some additional info, but not much.
WHat really happens when MODE is set to 10 and the code performs a pin high and then a pin low? For that info, one has to go to other ARM vendor documentation and hope that the ST works the same.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.