2015-12-07 9:24 AM
Hi to all,
I realized my first pcb using a STM32F030K6 MCU. The project is a very simple one, that is no external oscillator, only two leds and a usart interface.I can regularly download the program using ''flash loader demonstrator'' and leds blink as they should do. The problem is power consumption, that is 500 mA and, in fact, I needed to add a heath sink. I tried with another mcu, but the result was the same. I aspected no more tahn 20 mA and I do not understand where is the problem I looked on internet, but projects I found were similar to mine. Someone can help me? Thank youu Freya2015-12-07 10:26 AM
The problem is power consumption, that is 500 mA
Kind of screams of a short or conduction path.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.