2020-07-29 5:35 AM
The Project was migrated from STM32L4 to STM32L5. The Baudrate setting with HAL_UART_Init() works fine with L4 MCU. With L5 MCU it returns with an HAL_UART_ERROR_NONE too.
2020-07-29 6:06 AM
It should set BRR based on the current clocking options. Here it would typically unpack the RCC and PLL settings for clocks and buses.
You could debug or validate it is checking all the right bits, and using the right values.
The define for HSE_VALUE can be particularly problematic if wrong.
New STM32 also have more complex peripheral clock sourcing options, check those are being unpacked properly. Library source is available and can be inspected.
2020-07-29 6:52 AM
HAL_UART_ERROR_NONE = 0 = HAL_OK.
This indicates there is no error.
What issue are you running into? HAL_UART_Init does indeed calculate BRR based on your current clock settings.
2020-07-29 8:02 AM
Thanks for the quick and good comments,
@TDK
The issue is that the UART just did not recognize the incomming Data with a BRR setting of 0x42 (Set by HAL_UART_Init() Call)
Using the Formulaes I got a BRR=0x73 and the UART recognizes incoming Data correct. In this case the BRR ist overwritten after
call of HAL_UART_Init().
@Community member
HSE_VALUE seems to be the problem. I found a wrong define for this. The problem is not solved yet, but I think I'm on good way.
I was not aware that the calculations could depend on a user define.
Best regards
PKM
2020-07-29 8:15 AM
Well it is how the software knows what external hardware you've added, it doesn't know if you built a system with an 8 MHz clock or a 24 MHz one. It knows what the HSI / MSI are.
Typically in stm32l5xx_hal_conf.h
2020-07-29 8:49 AM
If the HAL function would get as passing parameter the incoming USART clock frequency in Hz would make backtracking simpler.
2020-07-30 1:39 AM
Hi,
Problem is solved.
The wrong Definition of the "HSE_VALU"E was as mentionend by clive1 in "stm32l5xx_hal_conf.h", but the file "system_stm32l5xx.c" had to be changed in the same way.
Thanks very much.
2020-07-30 5:40 AM
PLL settings would need to reflect board/design
HSE_VALUE you be used here too, but the math/best-fit is more difficult due to the limited options and integers
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.