2018-04-05 10:39 AM
Hi, everyone!
I am quite new to SSL/TLS and I am trying to make SSL server on my own STM32F427 MCU board. I already have the standard HTTP server working correctly using lwIP netconn library and I now am trying to make it be more secured with adding the SSL layer over same lwIP.
So, I am using the code source from CubeMX examples for SSL server, but always have the same problem with mbedtls_net_bind command execution. Seems that my code is exactly the same as in example, but at mine the mbedtls_net_bind function always returns value MBEDTLS_ERR_NET_SOCKET_FAILED.
I am setting MBEDTLS library for default values in STM32CubeMX and here are few things from code how I am doing the job:
1. Start of my SSL server code:
static mbedtls_net_context listen_fd;
mbedtls_net_init(&listen_fd);
// This function always gives out -0x42, which is MBEDTLS_ERR_NET_SOCKET_FAILED
if ((ret = mbedtls_net_bind(&listen_fd, NULL, '4433', MBEDTLS_NET_PROTO_TCP)) != 0)
{ debug_printf(' failed ! mbedtls_net_bind returned %d', ret); goto exit;}2. Function mbedtls_net_init:
void mbedtls_net_init( mbedtls_net_context *ctx )
{ctx->fd = -1;
// Check whether lwIP was already initialized
if (lwIpInitialized == 1) return;MX_LWIP_Init();
}3. Start of function mbedtls_net_bind, which is calling the problem:
int mbedtls_net_bind( mbedtls_net_context *ctx, const char *bind_ip, const char *port, int proto )
{ int ret = 0;int n;
struct addrinfo hints, *addr_list, *cur;/* Bind to IPv6 and/or IPv4, but only in the desired protocol */
memset( &hints, 0, sizeof( hints ) ); hints.ai_family = AF_UNSPEC; hints.ai_socktype = proto == MBEDTLS_NET_PROTO_UDP ? SOCK_DGRAM : SOCK_STREAM; hints.ai_protocol = proto == MBEDTLS_NET_PROTO_UDP ? IPPROTO_UDP : IPPROTO_TCP; if( bind_ip == NULL ) hints.ai_flags = AI_PASSIVE;if( getaddrinfo( bind_ip, port, &hints, &addr_list ) != 0 )
return( MBEDTLS_ERR_NET_UNKNOWN_HOST );/* Try the sockaddrs until a binding succeeds */
ret = MBEDTLS_ERR_NET_UNKNOWN_HOST; for( cur = addr_list; cur != NULL; cur = cur->ai_next ) {// Here at socket() function I always have an error, I have the following values at
// cur->ai_family = AF_UNSPEC;
// cur->ai_socktype = SOCK_STREAM;
// cur->ai_protocol = IPPROTO_TCP;
ctx->fd = (int) socket( cur->ai_family, cur->ai_socktype, cur->ai_protocol );if( ctx->fd < 0 )
{ ret = MBEDTLS_ERR_NET_SOCKET_FAILED; continue; }..........
Can anyone please suggest what I am doing wrong?Thanks for any useful response...#socket #mbedtls #mbedtls_err_net_socket_failed2025-01-10 2:53 AM
Evgeniy, did you succeed with that problem? I faced the same error on calling function:
if ((ret = mbedtls_net_bind(&listen_fd, NULL, "443", MBEDTLS_NET_PROTO_TCP)) != 0) {
goto exit;
}
Got all examples from folder mbed_tls - they all failed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.