2011-08-10 1:55 PM
How much is there, really? And how much is really available?
The specs all say 16 mbit, but the part and the schematic show 32 mbit, or 4 MBytes. Looking into the code examples include with IAR EWARM, it seems only A0-A17 are assigned to the FSMC, which suggests only 256 KBytes?! However, in the debugger there appears to be 512 KBytes of actually usable memory! So, here are my questions: 1. How much memory is actually usable? 2. How do I set up access to all of it? Thanks!2011-08-10 5:31 PM
For the STM3220F-EVAL
http://www1.futureelectronics.com/doc/STMICROELECTRONICS/STM3220G-EVAL.pdf The straight SRAM has 18 address bits, and is 16-bits wide. ie 256Kwords or 512Kbytes or 4Mbits A0..17 are shifted versions of A1..18 It's access time is 55ns, so figure about 7 times slower than internal SRAM. For the STM3220G-EVAL http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/USER_MANUAL/DM00022972.pdf The straight SRAM has 21 address bits, and is 16-bits wide. ie 2048Kwords or 4096Kbytes or 32Mbits (CY7C1071DV33) A0..20 are shifted versions of A1..21 It's access time is 12ns, so figure about 2 times slower than internal SRAM. It might be fitted with a smaller, slower, or faster part. The IS61WV102416BLL-10MLI is a 1024Kword, 2048Kbyte, 16Mbit part. At 10ns it's still at least 2 cycles. http://www.issi.com/pdf/61WV102416ALL.pdf I suspect you'd program the pins to associate with the FSMC, and you'd program the FSMC with the geometry of the device.2011-08-11 4:24 AM
Aha!
The key point you made is contained in the phrase ''A0..17 are shifted versions of A1..18'' (and the related point for my board), which explains the 256K/512K discrepency I noticed. I am also willing to readily believe that the code samples are intentionally compatible with the older board with the smaller SRAM. In my confusion and rush to get out a question before leaving for the day, it didn't occur to me that they would have done that ''shifting''; it seems more natural to me to label the signals A1..18. But that's just me... Now, I've got to figure out how to get those extra address bits mapped... Thanks, Clive1!!! -Bob2011-08-11 7:31 AM
Yes, on things like the 68K we had to play games with the address pin names on the schematic depending on the parts and the bus widths. I suspect the STM32 with it's pin constraints, and to simplify the schematics, went with a more dynamic scheme. Just another thing to watch out for.
A quick dig around didn't find a good FSMC example, mostly ''too be implemented i next version'' Confirming to myself it was really a 55ns part, not a 5.5ns one http://www.issi.com/china/pdf/66WV25616ALL-BLL.pdfWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.