2022-11-16 2:30 AM
Hello, my NUCLEO-H723ZG is running at 550 MHz and using maximum 137.5 MHz TIM for DAC triggering but I want triggering faster than this so, can I use external clk with frequency more than 137.5 MHz?
2022-11-16 3:49 AM
Maximum DAC sample rate is abour 51.1Msps (limited by data transfer from memory to DAC).
Faster triggering is meaningless (why to trigger DAC conversions with the same value ?).
Another topic is limited slewrate and bandwidth of embedded DAC output buffer (if you are using it).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.