2023-11-17 11:54 AM
What is the maximum clock source frequency can I use as an external clock for timer?
I have a 20MHz source and PLL frequency made out of this source. The purpose - generate lower frequency pulses that synchronous to that 20MHz clock with controlled delay. I can get 100MHz, 120MHz, 140Mhz, 160 MHz out of that PLL for delay of less or more precision and would like to know what will I be able to get.
It could be easy made with FPGA, but since ST got such high speed MCU, I hope I can do it just with a MCU. MCU will be needed anyway.
Solved! Go to Solution.
2023-11-17 12:17 PM
from H563 ds:
2023-11-17 12:17 PM
from H563 ds:
2023-11-17 12:30 PM - edited 2023-11-17 12:31 PM
I see, 125MHz, than.
Thanks
2023-11-17 12:55 PM
But the TIM's on the STM32 aren't very flexible / functional at all.
Integer dividers, single counting element, 4 channels. Saturated by interrupts into the few hundred KHz
Ok for generating 4x 50 Hz Servo signals.
I'd imagine you could do something a lot better with a CPLD, and perhaps an adder circuit instead of a counter. ie simple phase adder for NCO / DDS
There is a clock domain synchronizer on the front end to get the input clock into the 150 MHz domain
2023-11-20 10:35 AM - edited 2023-11-20 11:12 AM
Played last Friday. With 100MHz for the beginning.
The main problem for my task - the trigger can't have a shorter period than the counting timer. I mean, if I use a PWM or one pulse output, for example, the trigger signal should come, at least, right after the pulse finished. Better with some delay after the pulse.
That means I have to use FPGA. CPLD like Altera MAX V would be great for my task, but Intel still have problems with its production, Xilinx/AMD does not have modern CPLDs. Tried to look into Lattice - small ones won't work for me, big ones are not much cheaper than small Spartan 7. And I never worked with Lattice yet.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.