2025-08-25 1:19 AM - last edited on 2025-08-25 1:31 AM by mƎALLEm
Akkording to AN3155, July 2025: "The highest tested baud rate (BHigh) is 115200."
Have tried with 921600 and that seems to work fine.
Is the recommodation from ST that not use above 115200?
Solved! Go to Solution.
2025-08-25 5:50 AM
Hello,
The feedback from our internal team:
When the USART used in the bootloader is in auto-baudrate mode, the max baudrate is 921600. But when the USART used is non auto-baudrate, in this case, 115200 is the max recommended.
We plan to clarify that in the documentation.
Does it answer your question?
2025-08-25 2:26 AM - edited 2025-08-25 2:35 AM
Hello,
I'm checking that internally and get back to you when I have any feedback.
(Internal ticket number 216214)
2025-08-25 5:50 AM
Hello,
The feedback from our internal team:
When the USART used in the bootloader is in auto-baudrate mode, the max baudrate is 921600. But when the USART used is non auto-baudrate, in this case, 115200 is the max recommended.
We plan to clarify that in the documentation.
Does it answer your question?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.