2015-03-26 7:01 AM
I was wondering what the negative input can be on an ADC pin.
We have an analog signal that can be very rare -38mV for a short moment. In the datasheet page 60 of the F411 i can only find Absolute maximum ratings: Input voltage on FT and TC pins VSS –0.3 So it looks I'm within the marge, is that correct ?2015-03-26 7:59 AM
...i can only find Absolute maximum ratings: Input voltage on FT and TC pins VSS –0.3
There is, at least in my F40x datasheet, and additional column ''Unit'', which says ''V''. That means -300mV, so -38mV is in limits. However, protective measures are probably advisable. For small and low power negative surges, a schottky diode might be sufficient.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.