2011-01-29 9:59 AM
Manual for Std Peripheral Drivers for STM32?
2011-05-17 5:23 AM
www.st.com/stm32-discovery routes to
http://www.st.com/internet/evalboard/product/250863.jsp Design Support Software & Development tools - Firmware (Bottom of Page) http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/stm32vldiscovery_package.zip Top level directory you'll find stm32f10x-an3268_fw.chm Now I'll note that the examples from the old library, included with Keil and IAR evals, might be a better starting point as there are more different code examples than for the VL. The VL only works at upto 24 MHz, so you'll have to watch that.2011-05-17 5:23 AM
Thanks clive1, but I already have that - it is the help for the VL Discovery firmware package, not the Standard Peripheral Library. That is not included in the VL Discovery firmware package. So does it exist, somewhere else?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.