2017-11-02 6:29 AM
Hi all,
i'm trying to customize html files that are hosted in a webserver running on my st32 nucleo f676zi with lwIP library.
The big issue is that i can't understand the correct usage of makefsdata script.
Actually, on a macbook, i call ./makefsdata and it works fine with html files, it generates a fsdata.c based on the folder on witch i have my html files.
But when i insert some .shtml files (SSI) the browser show me the pure html code without parsing it.
I think the problem should be on makefsdata script because with the original fsdata it works fine also with shtml files!
I found a .exe makefsdata here (
) but when it's running on windows 10 it crashes due to the missing of MSVCR100D.dll library that i'm not able to fix.Thanks in advance for the help.
2017-11-06 12:35 AM
Any suggestions? Thanks
2018-06-09 9:21 AM
>But when i insert some .shtml files (SSI) the browser show me the pure html code without parsing it.
edit the perl script and add the mime type for shtml
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.