2018-05-25 1:32 AM
Dear friends,
I am trying to config lwIP Netconn APIs to connect my board to the TCP/IP network using STM32F107RCt6 MCU and a DP83848CVV PHY. The only options that I change in configuration tab in CubeMX is to disable the DHCP server and enter the static IP address and I add another freeRTOS thread with default stack size of 128 words. I used the tcp echo server example provided by ST and copied the code to the new thread I created and I am sure my code is fine and works well and when I download the code, the board even doesn't answer to the ICMP ping request!
I also tried to config the STM32F746 Discovery board but I get the same result and the board didn't answer to the ping request so I'm pretty sure there is something missing in my lwIP configuration in CubeMX.
I already run TCP echo server using STM32F107RCt6 with lwIP native raw apis version 1.3.1 and SPL libraries but I want to migrate to CubeMX and HAL libraries and new versions of lwIP and freeRTOS.
I would be very thankful if someone could help me in configurations. I am using the latest version of CubeMX and Keil IDE and lwIP version 2.0.0.
Solved! Go to Solution.
2018-05-25 4:59 AM
Hi
Hossaini.Mujtaba
,Try to set the PHY address to 0 and I increase the heap space in FreeRTOS by changing configTOTAL_HEAP_SIZE in FreeRTOS configuration.
Best Regards,
Imen
2018-05-25 2:10 AM
Hello
Hossaini.Mujtaba
,Did you set in the CubeMx the PHY address to 0 ?
With Regards,
Imen
2018-05-25 2:37 AM
Dear Imen,
Thanks for your quick reply.
The PHY address of my board is 1.
Best regards,
Mujtaba
2018-05-25 3:31 AM
Hi,
I will change the phy address but I dont think the problem lies within the freeRTOS because I couldnt ping the board even when I config lwIP to native raw api.
Thanks for your reply,
Mujtaba
2018-05-25 4:59 AM
Hi
Hossaini.Mujtaba
,Try to set the PHY address to 0 and I increase the heap space in FreeRTOS by changing configTOTAL_HEAP_SIZE in FreeRTOS configuration.
Best Regards,
Imen
2018-05-26 7:45 AM
Dear Imen,
I set the phy address to zero and I totally disabled FreeRTOS but still have the same problem.
The board does not even anser to the ping request.
Could you please give me a hint how I can find the problem?
As I said I coud run tcp echo server using lwip native raw api version 1.3.1 with phy address of 1 and spl libraries. (Without using cube the board worls well but when I use cube to do the initialaztions, the board does not work and I am 100% sure that the problem lies somewhere inside my lwip configurations in cube.)
Besr regards,
Mujtaba
2018-05-27 3:51 AM
Dear Imen,
Thanks for your help.
When I increased the total heap size of FreeRTOS, I could ping the board successfully.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.