2018-05-25 4:45 AM
Background
(note I asked this question too at
, but no answers yet).I am trying to make a SPI connection between two STM32F103C8T6's.
Measurements
According to my logic analyzer I get a signal that looks ok (sending 10 bytes with values 0x55):
Results
My receiver's callback function for RX Complete also stops in the breakpoint (last line in code below):
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{ /* Prevent unused argument(s) compilation warning */ if (hspi1.RxXferCount == 10)Problem
I sent 10 bytes, however, the RxXferCount has value 0. Instead, RxXferSize has value 10, but pRxBuffPtr is empty.
Question
How can I receive the correct bytes?
**Values from the register SPI1 and variable hspi1**
https://i.stack.imgur.com/xb5X5.png
Relevant code
Initialization (using a GPIO for defining Master and Slave):
/* SPI1 init function */
static void MX_SPI1_Init(void) { hspi1.Instance = SPI1; hspi1.Init.Mode = (HAL_GPIO_ReadPin(GPIOB, GPIO_PIN_12) == GPIO_PIN_SET ? SPI_MODE_MASTER : SPI_MODE_SLAVE); hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLE; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi1.Init.CRCPolynomial = 10; if (HAL_SPI_Init(&hspi1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); } } Main function:int main(void)
{ ... MX_SPI1_Init(); ..._transmitter = (HAL_GPIO_ReadPin(GPIOB, GPIO_PIN_12) == GPIO_PIN_SET ?
SPI_MODE_MASTER : SPI_MODE_SLAVE); while (1) { if (_transmitter) { uint8_t data[] = { 0x55, 0x55, 0x55, 0x55, 0x55, 0x55, 0x55, 0x55, 0x55, 0x55 }; HAL_SPI_Transmit_IT(&hspi1, data, 10); } else { HAL_SPI_Receive_IT(&hspi1, _spi_data, 10); } } }Solved! Go to Solution.
2018-05-27 3:46 AM
The problem has been 'solved'... Or better said, there was no problem in the first place. I expected the results (received data) to be in the variable
hspi in the interrupt handler, however, it is directly stored in the variable
_spi_data (passed during the receive call). And hspi is cleared up already while in the interrupt handler.
@T J I saw your comment has been removed; thanks for your reaction though.
2018-05-27 3:46 AM
The problem has been 'solved'... Or better said, there was no problem in the first place. I expected the results (received data) to be in the variable
hspi in the interrupt handler, however, it is directly stored in the variable
_spi_data (passed during the receive call). And hspi is cleared up already while in the interrupt handler.
@T J I saw your comment has been removed; thanks for your reaction though.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.