2025-02-13 4:46 AM
Hi everyone,
We’re working with the STM32H730 microcontroller and have a test setup for displaying content on a screen using LTDC. The test currently fills a buffer in external RAM, which is configured on internal flash memory. The result is as expected, and everything works fine.
For this, we have configured the OctoSPI (Octo2 mode) in HyperRAM mode and set up the necessary peripherals such as LTDC, DMA2D, and others.
Now, we want to replicate the same test, but this time using the external Flash memory. We already have control over the jump to the external flash, as we are developing code that executes from there. However, when we attempt to replicate the test, we encounter noise and distortion on the screen.
This raises several questions for us:
Any advice or insights would be greatly appreciated!
2025-02-24 2:03 AM - edited 2025-02-24 2:04 AM
Hello @HispaEmo,
Are you doing animation buffers on external memory?
Could you please give more details about LTDC reference, the LTDC and the OCTOSPI clocks frequencies?
May be these MOOCs can help you.
- STM32 Graphics: How to set up a different OSPI flash memory in a TouchGFX template, Part 1
- STM32 Graphics: How to set up a different OSPI flash memory in a TouchGFX template, Part 2
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.