2020-04-03 7:49 AM
Hello,
I'm using the STM32H750VB and want to use the LPTIM1 to wakeup for CSTOP.
But i'm not able to let the LPTIM1 run.
Code:
SysInt_RegisterIsr(WAKEUP_PIN_IRQn, WakeUpPinInterrupt);
SysInt_SetPriority(WAKEUP_PIN_IRQn, 1, 0);
SysInt_EnableIsr(WAKEUP_PIN_IRQn);
SysInt_RegisterIsr(LPTIM1_IRQn, LowPowerTimerInterupt);
SysInt_SetPriority(LPTIM1_IRQn, 0, 0);
SysInt_EnableIsr(LPTIM1_IRQn);
LSI_ClockEnable();
/* ### - 1 - Re-target the LSI to Clock the LPTIM Counter ################# */
/* Select the LSI clock as LPTIM peripheral clock */
RCC_PeriphCLKInitStruct.PeriphClockSelection = RCC_PERIPHCLK_LPTIM1;
RCC_PeriphCLKInitStruct.Lptim1ClockSelection = RCC_LPTIM1CLKSOURCE_LSI;
HAL_RCCEx_PeriphCLKConfig(&RCC_PeriphCLKInitStruct);
LptimHandle.Instance = LPTIM1;
LptimHandle.Init.Clock.Source = LPTIM_CLOCKSOURCE_APBCLOCK_LPOSC;
LptimHandle.Init.Clock.Prescaler = LPTIM_PRESCALER_DIV16;
LptimHandle.Init.Trigger.Source = LPTIM_TRIGSOURCE_0;
LptimHandle.Init.Trigger.ActiveEdge = LPTIM_ACTIVEEDGE_RISING;
LptimHandle.Init.CounterSource = LPTIM_COUNTERSOURCE_INTERNAL;
LptimHandle.Init.Input1Source = LPTIM_INPUT1SOURCE_GPIO;
LptimHandle.Init.Input2Source = LPTIM_INPUT2SOURCE_GPIO;
/* Initialize LPTIM peripheral according to the passed parameters */
HAL_LPTIM_Init(&LptimHandle);
/* Period = 65535
* Pulse = 32767
* According to this configuration (LPTIMER clocked by LSI & compare = 32767,
* the Timeout period = (compare + 1)/LSI_Frequency = 1s
*/
HAL_LPTIM_TimeOut_Start_IT(&LptimHandle, 0xFFFF, 0x8000);
2020-04-03 8:43 AM
Enable the clock with __HAL_RCC_LPTIM1_CLK_ENABLE before you use the peripheral.
2020-04-03 11:40 AM
Hey, thank you for the remark, but i already do this at startup:
/* ## - 1 - Enable LPTIM clock ############################################ */
__HAL_RCC_LPTIM1_CLK_ENABLE();
/* ## - 2 - Force & Release the LPTIM Periheral Clock Reset ############### */
/* Force the LPTIM Periheral Clock Reset */
__HAL_RCC_LPTIM1_FORCE_RESET();
/* Release the LPTIM Periheral Clock Reset */
__HAL_RCC_LPTIM1_RELEASE_RESET();
2020-04-03 12:03 PM
i checked this registers:
2020-08-19 3:38 PM
I had similar issue as that of MVanb.1. TDK's comment helped me a lot. Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.