2020-04-29 5:20 AM
Is there an LL example to enable the backup ram.
This doesn't work:
// Enable PWR clock
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);
// Enable Backup ram clock
LL_APB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_BKPSRAM);
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_RTCAPB);
// Enable backup ram regulator
LL_PWR_EnableBkUpAccess();
LL_PWR_EnableBkUpRegulator();
while (LL_PWR_IsActiveFlag_BRR() == 0);
*(__IO uint32_t *) (BKPSRAM_BASE ) = 0x5A5A5A5A;
I can't find in the documentation what I forgot.
Thanks.
2020-05-04 2:14 AM
I changed my code to this:
void CPU_config_backupram(void)
{
volatile uint32_t test;
RCC->APB1ENR |= 0x10000000;
PWR->CR1 |= 0x00000100;
RCC->AHB1ENR |= 0x00040000;
test = PWR->CSR1;
PWR->CSR1 |= 0x00000200;
while( (PWR->CSR1 & 0x00000008) != 0x00000008) ;
test = PWR->CSR1;
}
PWR->CSR1 is still 0x34000.
So are there any other requirements?
Reading variable: test gives me the following error message:
Multiple errors reported.
1) Failed to execute MI command:
-var-create - * test
Error message from debugger back end:
-var-create: unable to create variable object
2) Unable to create variable object
3) Failed to execute MI command:
-data-evaluate-expression test
Error message from debugger back end:
No symbol "test" in current context.
4) Failed to execute MI command:
-var-create - * test
Error message from debugger back end:
-var-create: unable to create variable object
2020-05-04 2:17 AM
To the only code other execute before CPU_config_backupram is STM32F767ZITX_FLASH.ld and this function is this:
void SystemClock_Config(void)
{
/* Enable HSE clock */
LL_RCC_HSE_EnableBypass();
LL_RCC_HSE_Enable();
while(LL_RCC_HSE_IsReady() != 1)
{
};
/* Set FLASH latency */
LL_FLASH_SetLatency(LL_FLASH_LATENCY_7);
/* Enable PWR clock */
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);
/* Activation OverDrive Mode */
LL_PWR_EnableOverDriveMode();
while(LL_PWR_IsActiveFlag_OD() != 1)
{
};
/* Activation OverDrive Switching */
LL_PWR_EnableOverDriveSwitching();
while(LL_PWR_IsActiveFlag_ODSW() != 1)
{
};
/* Main PLL configuration and activation */
LL_RCC_PLL_ConfigDomain_SYS(LL_RCC_PLLSOURCE_HSE, LL_RCC_PLLM_DIV_8, 432, LL_RCC_PLLP_DIV_2);
LL_RCC_PLL_Enable();
while(LL_RCC_PLL_IsReady() != 1)
{
};
/* Sysclk activation on the main PLL */
LL_RCC_SetAHBPrescaler(LL_RCC_SYSCLK_DIV_1);
LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL);
while(LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_PLL)
{
};
/* Set APB1 & APB2 prescaler */
LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_4);
LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_2);
/* Update CMSIS variable (which can be updated also through SystemCoreClockUpdate function) */
SystemCoreClock = 216000000;
}
2020-05-04 2:28 AM
RCC->APB1ENR |= 0x10000000;
PWR->CR1 |= 0x00000100;
RCC->AHB1ENR |= 0x00040000;
test = PWR->CSR1;
PWR->CSR1 |= 0x00000200;
while( (PWR->CSR1 & 0x00000008) != 0x00000008) ;
test = PWR->CSR1;
This solved the problem. Somehow the debug environment uses an other image with the new source code?
2020-05-04 2:29 AM
All bus prescalers should be changed before increasing frequency. Why do you set APB1 and APB2 after the clock change?
2020-05-04 2:31 AM
Copied this from an UART example. So I assumed it worked correctly. So please tell me how it is done correctly.
2020-05-04 3:07 AM
This seems the correct low level driver code for configure the backup ram:
void CPU_config_backupram(void)
{
// Enable PWR clock
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);
// Enable Backup ram clock
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_BKPSRAM);
// Enable backup ram regulator
LL_PWR_EnableBkUpAccess();
LL_PWR_EnableBkUpRegulator();
while (LL_PWR_IsActiveFlag_BRR() == 0);
}
2020-05-04 3:08 AM
I literally told you it in my previous post!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.