2020-04-29 5:20 AM
Is there an LL example to enable the backup ram.
This doesn't work:
// Enable PWR clock
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);
// Enable Backup ram clock
LL_APB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_BKPSRAM);
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_RTCAPB);
// Enable backup ram regulator
LL_PWR_EnableBkUpAccess();
LL_PWR_EnableBkUpRegulator();
while (LL_PWR_IsActiveFlag_BRR() == 0);
*(__IO uint32_t *) (BKPSRAM_BASE ) = 0x5A5A5A5A;
I can't find in the documentation what I forgot.
Thanks.
2020-04-30 7:57 AM
Hello,
I don't know which product you are using precisely.
But the STM32CubeF7 package proposes the Example RTC_Tamper with the following purpose: "Configuration of the RTC HAL API to write/read data to/from RTC Backup registers."
You can download the package here:
It is available for the boards STM32756G_EVAL, STM32F769I_EVAL, STM32F746ZG-Nucleo but there should be no problem to adapt it for your F7.
The example path is for example STM32Cube_FW_F7_V1.16.0\Projects\STM32756G_EVAL\Examples\RTC\RTC_Tamper
Hope it will help.
Adam S.
2020-05-01 12:30 AM
I'm using the Nucleo-F676ZI
LL_PWR_EnableBkUpAccess();
LL_RTC_BAK_SetRegister(RTC, LL_RTC_BKP_DR1, 10);
Power Cycle:
uint32_t data1 = LL_RTC_BAK_GetRegister(RTC, LL_RTC_BKP_DR1);
works fine. So this that is not the problem and the backup supply and regulator works correctly.
LL_PWR_EnableBkUpAccess();
for(i=0;i<10;i++)
{
*(__IO uint8_t *) (BKPSRAM_BASE+ i) = i;
}
SCB_CleanDCache_by_Addr ((uint32_t *)BKPSRAM_BASE, BKPSRAM_SIZE);
In memory browser I see the memory is correctly written. After a reset cycle I can read the data correct back.
Only after a power cycle all the data is lost.
I excluded CPU_CACHE_Enable from my program. I use the default LL driver STM32F767ZITX_FLASH.ld and initialization functions.
So some detailed information how to use the Backup ram or a backup ram example should be nice.
Thanks!
2020-05-01 1:30 AM
> In memory browser I see the memory is correctly written.
On what address?
JW
> I'm using the Nucleo-F676ZI
A new model, yummy! ;)
2020-05-01 2:42 AM
Nucleo-F767ZI
#define BKPSRAM_BASE 0x40024000UL /*!< Base address of : Backup SRAM(4 KB) */
from stm32f767xx.h
2020-05-01 2:54 AM
Write backup ram
reset.
Breakpoint after enables breakup sram clock
Power cycle.
Again breakpoint after enabling breakup sram clock
2020-05-02 3:22 PM
Humm, and PWR_CSR1 content at both of these situations?
Also, RTC runs uninterrupted during the power outage, i.e. if it's say a minute long, the RTC time is not delayed?
JW
2020-05-03 11:00 PM
PWR_CSR1 is in both situation 0x34000.
I don't use the RTC. I only need the backup ram.
2020-05-03 11:34 PM
Hello,
So it seems that there is a problem with this part of your code:
LL_PWR_EnableBkUpRegulator();
while (LL_PWR_IsActiveFlag_BRR() == 0);
Because bit 9 (BRE Backup regulator enable) of PWR_CSR1 is not setif its value is 0x34000.
PWR-CR1 should be 0x34200 even after a power cycle
Could you try to set it manually with PWR->CSR1 = 0x00034200,
And check that bit 9 has not been reset after power cycle ?
2020-05-04 12:10 AM
PWR->CSR1 = 0x00034200;
don't change the value of CR1 after this the value is still 0x34000
I also tried this:
LL_PWR_EnableBkUpAccess();
PWR->CSR1 = 0x00034200;
Still the CR1 is not updated.
2020-05-04 1:07 AM
The following code works for me (i used the f746 discovery board but the register mapping is the same for f76x products).
PWR->CR1 is well updated after the while (test is a global variable).
RCC->APB1ENR |= 0x10000000;
PWR->CR1 |= 0x00000100;
RCC->AHB1ENR |= 0x00040000;
test = PWR->CSR1;
PWR->CSR1 |= 0x00000200;
while( (PWR->CSR1 & 0x00000008) != 0x00000008) ;
test = PWR->CSR1;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.