2020-06-04 10:07 AM
hi
i have simple code for send some data from one master 767 to other slave
in master data will send in 2khz rate and 80 byte length
but data in slave not completely correct on Rx buffer one data ok and next not, until end of buffer that repeated (for example rx buff is=[0,129,1,130,2,131,3......])
slave (rx mcu) code
#define RxLen 80
void SPI4_RxCplt(void);
uint8_t RxBuffer[100];
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_TIM2_Init();
MX_SPI4_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
static void MX_SPI4_Init(void)
{
/* USER CODE BEGIN SPI4_Init 0 */
/* USER CODE END SPI4_Init 0 */
LL_SPI_InitTypeDef SPI_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Peripheral clock enable */
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI4);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOE);
/**SPI4 GPIO Configuration
PE2 ------> SPI4_SCK
PE5 ------> SPI4_MISO
PE6 ------> SPI4_MOSI
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_2;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOE, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_5;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOE, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_6;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/* SPI4 DMA Init */
/* SPI4_RX Init */
LL_DMA_SetChannelSelection(DMA2, LL_DMA_STREAM_0, LL_DMA_CHANNEL_4);
LL_DMA_SetDataTransferDirection(DMA2, LL_DMA_STREAM_0, LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
LL_DMA_SetStreamPriorityLevel(DMA2, LL_DMA_STREAM_0, LL_DMA_PRIORITY_VERYHIGH);
LL_DMA_SetMode(DMA2, LL_DMA_STREAM_0, LL_DMA_MODE_CIRCULAR);
LL_DMA_SetPeriphIncMode(DMA2, LL_DMA_STREAM_0, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetMemoryIncMode(DMA2, LL_DMA_STREAM_0, LL_DMA_MEMORY_INCREMENT);
LL_DMA_SetPeriphSize(DMA2, LL_DMA_STREAM_0, LL_DMA_PDATAALIGN_BYTE);
LL_DMA_SetMemorySize(DMA2, LL_DMA_STREAM_0, LL_DMA_MDATAALIGN_BYTE);
LL_DMA_DisableFifoMode(DMA2, LL_DMA_STREAM_0);
/* USER CODE BEGIN SPI4_Init 1 */
/* USER CODE END SPI4_Init 1 */
/* SPI4 parameter configuration*/
SPI_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX;
SPI_InitStruct.Mode = LL_SPI_MODE_SLAVE;
SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_8BIT;
SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_LOW;
SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE;
SPI_InitStruct.NSS = LL_SPI_NSS_SOFT;
SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST;
SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
SPI_InitStruct.CRCPoly = 7;
LL_SPI_Init(SPI4, &SPI_InitStruct);
LL_SPI_SetStandard(SPI4, LL_SPI_PROTOCOL_MOTOROLA);
LL_SPI_DisableNSSPulseMgt(SPI4);
/* USER CODE BEGIN SPI4_Init 2 */
LL_DMA_ConfigAddresses(DMA2, LL_DMA_STREAM_0, LL_SPI_DMA_GetRegAddr(SPI4), (uint32_t)RxBuffer,
LL_DMA_GetDataTransferDirection(DMA2, LL_DMA_STREAM_0));
LL_DMA_SetDataLength(DMA2, LL_DMA_STREAM_0, RxLen);
LL_DMA_SetChannelSelection(DMA2, LL_DMA_STREAM_0, LL_DMA_CHANNEL_4);
LL_DMA_EnableIT_TC(DMA2, LL_DMA_STREAM_0);
LL_SPI_EnableDMAReq_RX(SPI4);
LL_DMA_ClearFlag_TC0(DMA2);
LL_SPI_Enable(SPI4);
LL_DMA_EnableStream(DMA2, LL_DMA_STREAM_0);
/* USER CODE END SPI4_Init 2 */
}
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA2_CLK_ENABLE();
/* DMA interrupt init */
/* DMA2_Stream0_IRQn interrupt configuration */
NVIC_SetPriority(DMA2_Stream0_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
NVIC_EnableIRQ(DMA2_Stream0_IRQn);
}
void SPI4_RxCplt(void)
{
// LL_DMA_DisableStream(DMA2, LL_DMA_STREAM_3);
HAL_GPIO_TogglePin(LED1_GPIO_Port,LED1_Pin);
}and master (Tx mcu)
#define TxLen 80
void SPI1_TxCplt(void);
uint8_t TxBuffer[100];
int main(void)
{
MX_GPIO_Init();
MX_DMA_Init();
MX_SPI1_Init();
MX_TIM2_Init();
/* USER CODE BEGIN 2 */
for (uint8_t i=0;i<100;i++)
{
TxBuffer[i]=i;
}
HAL_TIM_Base_Start_IT(&htim2);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if(htim->Instance==TIM2)
{
LL_DMA_EnableStream(DMA2, LL_DMA_STREAM_3);
}
/* USER CODE END 3 */
}
static void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
LL_SPI_InitTypeDef SPI_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Peripheral clock enable */
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI1);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA);
/**SPI1 GPIO Configuration
PA5 ------> SPI1_SCK
PA6 ------> SPI1_MISO
PA7 ------> SPI1_MOSI
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_5;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_6;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_7;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* SPI1 DMA Init */
/* SPI1_TX Init */
LL_DMA_SetChannelSelection(DMA2, LL_DMA_STREAM_3, LL_DMA_CHANNEL_3);
LL_DMA_SetDataTransferDirection(DMA2, LL_DMA_STREAM_3, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
LL_DMA_SetStreamPriorityLevel(DMA2, LL_DMA_STREAM_3, LL_DMA_PRIORITY_VERYHIGH);
LL_DMA_SetMode(DMA2, LL_DMA_STREAM_3, LL_DMA_MODE_CIRCULAR);
LL_DMA_SetPeriphIncMode(DMA2, LL_DMA_STREAM_3, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetMemoryIncMode(DMA2, LL_DMA_STREAM_3, LL_DMA_MEMORY_INCREMENT);
LL_DMA_SetPeriphSize(DMA2, LL_DMA_STREAM_3, LL_DMA_PDATAALIGN_BYTE);
LL_DMA_SetMemorySize(DMA2, LL_DMA_STREAM_3, LL_DMA_MDATAALIGN_BYTE);
LL_DMA_DisableFifoMode(DMA2, LL_DMA_STREAM_3);
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
SPI_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX;
SPI_InitStruct.Mode = LL_SPI_MODE_MASTER;
SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_8BIT;
SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_LOW;
SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE;
SPI_InitStruct.NSS = LL_SPI_NSS_SOFT;
SPI_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV2;
SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST;
SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
SPI_InitStruct.CRCPoly = 7;
LL_SPI_Init(SPI1, &SPI_InitStruct);
LL_SPI_SetStandard(SPI1, LL_SPI_PROTOCOL_MOTOROLA);
LL_SPI_EnableNSSPulseMgt(SPI1);
/* USER CODE BEGIN SPI1_Init 2 */
LL_DMA_ClearFlag_TC3(DMA2);
LL_DMA_ConfigAddresses(DMA2, LL_DMA_STREAM_3, (uint32_t)TxBuffer, LL_SPI_DMA_GetRegAddr(SPI1),
LL_DMA_GetDataTransferDirection(DMA2, LL_DMA_STREAM_3));
LL_DMA_SetDataLength(DMA2, LL_DMA_STREAM_3, TxLen);
// LL_DMA_SetChannelSelection(DMA2, LL_DMA_STREAM_3, LL_DMA_CHANNEL_3);
LL_DMA_EnableIT_TC(DMA2, LL_DMA_STREAM_3);
LL_SPI_EnableDMAReq_TX(SPI1);
LL_DMA_ClearFlag_TC3(DMA2);
LL_SPI_Enable(SPI1);
/* USER CODE END SPI1_Init 2 */
}
void SPI1_TxCplt(void)
{
// LL_SPI_Disable(SPI1);
LL_DMA_DisableStream(DMA2, LL_DMA_STREAM_3);
}
2020-06-04 11:01 AM
What can be seen on the line, i.e. is this problem of transmitter or receiver?
JW
2020-06-04 12:08 PM
in receiver.
transmit data is [0,1,2,3,4,....]
receive data is [0,129,1,130,2,131,3,....]
2020-06-04 12:21 PM
Did you observe the SCK and MOSI lines using oscilloscope or logic analyzer?
Without that, you can't conclude where is the problem.
You can try to bit-bang the transmitter, that's quite easy.
JW
2020-06-04 1:09 PM
my mcu s is on pcb and there isn't any test point for that signals
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.