2011-11-15 3:33 AM
I need( from some reason) to get always the same size of bin file.
I've tried to create other flash-section and fill it with some value.As last section I added following...added :
{
FILL(0xAB);
. = ALIGN(0x20000) - 1; //128kB
BYTE(0xAB); //write something to say linker its really section
} >FLASH
But than original linker script continue with/* used by the startup to initialize data */
_sidata = .;
/* Initialized data sections goes into RAM, load LMA copy after code */ .data : AT ( _sidata ) { . = ALIGN(4); _sdata = .; /* create a global symbol at data start */ *(.data) /* .data sections */ *(.data*) /* .data* sections */ . = ALIGN(4); _edata = .; /* define a global symbol at data end */ } >RAMSo my bin file doesnt finished at 0x8020000 but continue with _sidata.When I switch_sidata = .;
with my added section, I get error.
overlaps section .added loaded at [08010694,0801ffff]
#linker-stm32We’re moving the ST Community to a new platform to give you a better and more reliable community experience.