2008-10-28 3:39 AM
LED blink Performancestick
2011-05-17 3:48 AM
Does anyone have a simple example of an LED blink for the Performance Stick? I'm just looking for a simple piece of code in C that initializes the I/O without the libraries. I tend to avoid the libraries and roll my own code and this is the best way for me to get started.
2011-05-17 3:48 AM
Since I haven't had any responses from the forum I thought I would post an example I wrote for the LM3S317 from Luminary micro. The ST micro reference manual doesn't give a procedure for initializing peripherals so I'm looking for an example.
/ LEDblink.c for the LM3S317 //Declare functions int main(void); void dummy_handler(void); void isrPWM0(void); //Define the vector table __attribute__ ((section(''vectors''))) int const VectorStackTop = 0x20000800; // Exception 0, Starting value of MSP __attribute__ ((section(''vectors''))) int (* const VectorMain) (void) = main; // Exception 1, Reset __attribute__ ((section(''vectors''))) int (* const VectorMNI) (void) = main; // Exception 2, NMI __attribute__ ((section(''vectors''))) void (* const VectorArray[]) (void) = { dummy_handler, // Exception 3, hard fault dummy_handler, // Exception 4, MemManage fault dummy_handler // Exception 5, Bus fault }; //Dummy Handler void dummy_handler(void) { return; } //***************************************************************************** // Declarations //***************************************************************************** // Macro for Register access #define HWREG(x) (*((volatile unsigned long *)(x))) // System Control Registers #define SYSCTL_BASE 0x400FE000 //Base address #define RCGC2 HWREG(SYSCTL_BASE+0x0108) // GPIO Registers #define GPIOD 1<#define GPIO_PORTD 0x40007000 #define GPIODATA_OFFSET 0x03FC //Data for 255 <#define GPIODIR_OFFSET 0x0400 #define GPIODEN_OFFSET 0x051C #define PDDATA HWREG(GPIO_PORTD+GPIODATA_OFFSET) #define PDDIR HWREG(GPIO_PORTD+GPIODIR_OFFSET) #define PDDEN HWREG(GPIO_PORTD+GPIODEN_OFFSET) //Port Pins #define P2 1<//***************************************************************************** // Initialize LED //***************************************************************************** void initLED (void) { RCGC2 |=GPIOD; //Enable Port D clocking PDDIR |=P2; //Port D pin 2 output PDDEN |=P2; //Port D pin 2 digital enable } //***************************************************************************** // LED on //***************************************************************************** void LEDon (void) { PDDATA &= (~P2); } //***************************************************************************** // LED off //***************************************************************************** void LEDoff (void) { PDDATA |=P2; } //***************************************************************************** // Main //***************************************************************************** int main(void) { volatile unsigned long ulLoop; initLED(); //Set up LED port while(1) { for(ulLoop = 0; ulLoop < 0x10000; ulLoop++) { } LEDon(); for(ulLoop = 0; ulLoop < 0x10000; ulLoop++) { } LEDoff(); } }2011-05-17 3:48 AM
Well, I'd say it has to do with the fact that you specifically asked for code that does not make use of the libraries. If there's a library that makes life easier for you - why not use it?
2011-05-17 3:48 AM
The short answer:
I'm concerned with the ''how'' not the ''why'' The long answer: There was a thread a while back about a guy that wanted to write in assembly. I've only evolved one step beyond this person in that I use C to get away from the mechanics of assembly language and to make my code a little more readable. But I still come from an assembly code and hardware design background and I like to have control over the mcu at the register level.2011-05-17 3:48 AM
I don't know what port the performance stick led is on, or whether it is push-pull or open-drain, but this (untested code) ought to toggle PB10 in push-pull mode.
typedef unsigned long u32; #define RCC_ABP2ENR *((u32*)0x40021018) #define GPIOB_CRH *((u32*)0x40010C04) #define GPIOB_ODR *((u32*)0x40010C0C) int main(void) { RCC_ABP2ENR |= 0x8; // enable GPIOB in RCC_ABP2ENR GPIOB_CRH = 0x00000300; // set PB10 to output push pull u32 Delay; while(1) { GPIOB_ODR = (1 << 10); // turn on PB10 in GPIOB_ODR for (Delay = 0; Delay < 500000; Delay++); GPIOB_ODR = 0; // turn off PB10 in GPIOB_ODR for (Delay = 0; Delay < 500000; Delay++); } } [ This message was edited by: paul.smitton on 28-10-2008 09:56 ]2011-05-17 3:48 AM
That is very helpful.
Thanks!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.