2018-04-15 9:38 AM
so i was simply trying to test a touche in a specifique spot like this :
if(TS_State.touchDetected)
{ /* Get X and Y position of the touch post calibrated */ x = TS_State.touchX[0]; y = TS_State.touchY[0]; radius = TS_State.touchWeight[0]/3; LCD_UsrLog (' %d %d \r\n',x,y); if ((y > (45)) && (y < (51))) {if ((x > (430)) &&
(x < (435))) { LCD_UsrLog (' Fi blasetha \r\n'); }} }but it seems that it can't compare them to the numbers i used, but when i use the code from the example it works fine so _ i had to add or subb to get where i want, is there a better way ?
_ and if i click is keeps counting is it possible to count only one touche ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.