2018-07-09 12:04 AM
I have been teaching myself to user the STM32 MCUs.
I have done the usual blink and LED and create a Delay timer, setup a UART as a serial console for debugging.
I did also write a I2C software slave using and interrupt on the SDA line to detect the master sending a start condition.
I am now tring to use a LCD TFT in parallel using FSMC. I have tried both a ST7781 in 8 bit parallel and now a HX8357 in 16 bit parallel.
The FSCM seems to be working correctly as if I out my scope on any of the pins I see the output that I would expect but nothign shows up on the screen.
here's my code
#include 'stm32f4xx.h'
//used for coutn down in Delay__IO uint32_t TimmingDelay;void SysTick_Handler(void){ if(TimmingDelay !=0) { TimmingDelay --; }}void Delay(__IO uint32_t time){ TimmingDelay = time; while(TimmingDelay !=0);}//pointer used to write to start address of FSMCvolatile uint16_t* fsmc = (uint16_t*)0x60000000;void FSMC_setup(void){ //enable RCC for FSMC and both GPIO ports RCC->AHB3ENR |= RCC_AHB3ENR_FSMCEN; RCC->AHB1ENR |= RCC_AHB1ENR_GPIODEN | RCC_AHB1ENR_GPIOEEN; //setup RS (PD13) and RST (PD12) pin as output GPIOD->MODER |= GPIO_MODER_MODER13_0 | GPIO_MODER_MODER12_0; //setup other pins as AF GPIOD->MODER |= GPIO_MODER_MODER0_1 | GPIO_MODER_MODER1_1 | GPIO_MODER_MODER4_1 | GPIO_MODER_MODER5_1 | GPIO_MODER_MODER7_1 | GPIO_MODER_MODER8_1 | GPIO_MODER_MODER9_1 | GPIO_MODER_MODER10_1 | GPIO_MODER_MODER14_1 | GPIO_MODER_MODER15_1; GPIOE->MODER |= GPIO_MODER_MODER7_1 | GPIO_MODER_MODER8_1 | GPIO_MODER_MODER9_1 | GPIO_MODER_MODER10_1 | GPIO_MODER_MODER11_1 | GPIO_MODER_MODER12_1 | GPIO_MODER_MODER13_1 | GPIO_MODER_MODER14_1 | GPIO_MODER_MODER15_1; //setup pins as PP GPIOD->OTYPER = 0x00000000; GPIOE->OTYPER = 0x00000000; //set speed to 100MHz GPIOD->OSPEEDR = 0xFFFFFFFF; GPIOE->OSPEEDR = 0xFFFFFFFF; //set NO pull-up or pull-down GPIOD->PUPDR = 0x00000000; GPIOE->PUPDR = 0x00000000; //set other pins to AF12 i.e as FSMC pins GPIOD->AFR[0] |= (GPIO_AF12_FSMC << (0 * 4)) | (GPIO_AF12_FSMC << (1 * 4)) | (GPIO_AF12_FSMC << (4 * 4)) | (GPIO_AF12_FSMC << (5 * 4)) | (GPIO_AF12_FSMC << (7 * 4)); GPIOD->AFR[1] |= (GPIO_AF12_FSMC << ((8 - 8) * 4)) | (GPIO_AF12_FSMC << ((9 - 8) * 4)) | (GPIO_AF12_FSMC << ((10 - 8) * 4)) | (GPIO_AF12_FSMC << ((14 - 8) * 4)) | (GPIO_AF12_FSMC << ((15 - 8) * 4)); GPIOE->AFR[0] |= (GPIO_AF12_FSMC << (7 * 4)); GPIOE->AFR[1] |= (GPIO_AF12_FSMC << ((8 - 8) * 4)) | (GPIO_AF12_FSMC << ((9 - 8) * 4)) | (GPIO_AF12_FSMC << ((10 - 8) * 4)) | (GPIO_AF12_FSMC << ((11 - 8) * 4)) | (GPIO_AF12_FSMC << ((12 - 8) * 4)) | (GPIO_AF12_FSMC << ((13 - 8) * 4)) | (GPIO_AF12_FSMC << ((14 - 8) * 4)) | (GPIO_AF12_FSMC << ((15 - 8) * 4)); //setup FSMC on Bank1 NORSRAM1 //disable ASYNCWAIT: FSMC_Bank1->BTCR[0] &= ~FSMC_BCR1_ASYNCWAIT; //disable Extended mode FSMC_Bank1->BTCR[0] &= ~FSMC_BCR1_EXTMOD; //disable the wait for NWAIT signal FSMC_Bank1->BTCR[0] &= ~FSMC_BCR1_WAITEN; //write enable FSMC_Bank1->BTCR[0] |= FSMC_BCR1_WREN; //disable wrap mode FSMC_Bank1->BTCR[0] &= ~FSMC_BCR1_WRAPMOD; //disable Burst mode FSMC_Bank1->BTCR[0] &= ~FSMC_BCR1_BURSTEN; //enable Flash access FSMC_Bank1->BTCR[0] |= FSMC_BCR1_FACCEN; //set data bus width to 16 bit FSMC_Bank1->BTCR[0] |= FSMC_BCR1_MWID_0; //set to SRAM type FSMC_Bank1->BTCR[0] &= ~FSMC_BCR1_MTYP; //disable Address/data multiplexing FSMC_Bank1->BTCR[0] &= ~FSMC_BCR1_MUXEN; //enable Memory bank FSMC_Bank1->BTCR[0] |= FSMC_BCR1_MBKEN; //setup timings //set access mode A FSMC_Bank1->BTCR[1] &= ~FSMC_BTR1_ACCMOD; //set short bus turn around FSMC_Bank1->BTCR[1] &= ~(FSMC_BTR1_BUSTURN_0 | FSMC_BTR1_BUSTURN_1 | FSMC_BTR1_BUSTURN_2 |FSMC_BTR1_BUSTURN_3);}void TFT_write_cmd(uint16_t command){ //set RS pin low GPIOD->ODR &= ~GPIO_ODR_ODR_13; Delay(10); *fsmc = command; //set RS pin high GPIOD->ODR |= GPIO_ODR_ODR_13; Delay(10);}//sets up a HX8357B TFTvoid TFT_setup(void){ //hardware reset GPIOD->ODR &= ~GPIO_ODR_ODR_12; Delay(200); GPIOD->ODR |= GPIO_ODR_ODR_12; Delay(120); //software reset TFT_write_cmd(0x01); Delay(120); //sleep out TFT_write_cmd(0x11); Delay(120); //Normal Display Mode On) TFT_write_cmd(0x13); //Display On TFT_write_cmd(0x29); //CASET (Column Address Set) TFT_write_cmd(0x2A); *fsmc = 0000; *fsmc = 320; //PASET (Page Address Set) TFT_write_cmd(0x2B); *fsmc = 0000; *fsmc = 320; //Exit_idle_mode TFT_write_cmd(0x38); //Set_pixel_format RGR565 16 bit TFT_write_cmd(0x3A); *fsmc = 0b01010101; //RAMWR (Memory Write) TFT_write_cmd(0x2C);}void main(void){ // At this stage the system clock should have already been configured // at high speed. //set systick for 1 MS used in Delay interrupt SysTick_Config(SystemCoreClock/1000); FSMC_setup(); TFT_setup(); for (uint32_t i = 0; i < 102400; ++i ){ *fsmc = 0xff00; fsmc += 2; } // Infinite loop while (1){ // Add your code here. }}2018-07-12 2:42 AM
I have found solution to my setup FSMC problem.
Here is working setup
//setup timings of FSCM
FSMC_Bank1->BTCR[1] = FSMC_BTR1_ADDSET_1 | FSMC_BTR1_DATAST_1; // Bank1 NOR/SRAM control register configuration FSMC_Bank1->BTCR[0] = FSMC_BCR1_MWID_0 | FSMC_BCR1_WREN | FSMC_BCR1_MBKEN;We’re moving the ST Community to a new platform to give you a better and more reliable community experience.