2016-04-16 7:40 AM
Hi all,
I have trouble getting a LDC Display on the STM32F429 FMC to work in 8080 Mode. I use the same hardware connection like withe STMF4Discovery Expansion Board and the STM32F4DIS-LCD Modul.FMC_D0 (PD14) -> LCD_D0
FMC_D1 (PD15) -> LCD_D1 FMC_D2 (PD0) -> LCD_D2 FMC_D3 (PD1) -> LCD_D3 FMC_D4 (PE7) -> LCD_D4 FMC_D5 (PE8) -> LCD_D5 FMC_D6 (PE9) -> LCD_D6 FMC_D7 (PE10) -> LCD_D7 FMC_D8 (PE11) -> LCD_D8 FMC_D9 (PE12) -> LCD_D9 FMC_D10 (PE13) -> LCD_D10 FMC_D11 (PE14) -> LCD_D11 FMC_D12 (PE15) -> LCD_D12 FMC_D13 (PD8) -> LCD_D13 FMC_D14 (PD9) -> LCD_D14 FMC_D15 (PD10) -> LCD_D15 FMC_A0 (PF0) -> LCD_DC FMC_NOE (PD4) -> LCD_RD FMC_NWE (PD5) -> LCD_WR FMC_NE1 (Pd7) -> LCD_CS The Hardware configuration must be OK because I'm able to read out the correct ID of the SSD2119 Display Cotroller as 0x9919. But I have problems writing command and data to the display. When I compare the timing with a logic analyzer it seems that with the STM32F429 FMC the A0 address line is changed too late from command (low) to data (high) (see attached figure, marker B) compared to the working STMF4Discovery board which is equipped with a STM32F407 with a FSMC. It also seems the the data is put on the bus with the wrong endianess (please see attached figures). My FMC configuration:FMC_NORSRAMInitTypeDef FMC_NORSRAMInitStructure;
FMC_NORSRAMTimingInitTypeDef p; FMC_NORSRAMStructInit(&FMC_NORSRAMInitStructure); /*-- FSMC Configuration ------------------------------------------------------*/ /*----------------------- SRAM Bank 1 ----------------------------------------*/ /* FMC_Bank1_NORSRAM1 configuration */ p.FMC_AddressSetupTime = 7; p.FMC_AddressHoldTime = 7; p.FMC_DataSetupTime = 15; p.FMC_BusTurnAroundDuration = 15; p.FMC_CLKDivision = 15; p.FMC_DataLatency = 15; p.FMC_AccessMode = FMC_AccessMode_A; FMC_NORSRAMInitStructure.FMC_Bank = FMC_Bank1_NORSRAM1; FMC_NORSRAMInitStructure.FMC_DataAddressMux = FMC_DataAddressMux_Disable; FMC_NORSRAMInitStructure.FMC_MemoryType = FMC_MemoryType_SRAM; FMC_NORSRAMInitStructure.FMC_MemoryDataWidth = FMC_NORSRAM_MemoryDataWidth_16b; FMC_NORSRAMInitStructure.FMC_BurstAccessMode = FMC_BurstAccessMode_Disable; FMC_NORSRAMInitStructure.FMC_AsynchronousWait = FMC_AsynchronousWait_Disable; FMC_NORSRAMInitStructure.FMC_WaitSignalPolarity = FMC_WaitSignalPolarity_Low; FMC_NORSRAMInitStructure.FMC_WrapMode = FMC_WrapMode_Disable; FMC_NORSRAMInitStructure.FMC_WaitSignalActive = FMC_WaitSignalActive_BeforeWaitState; FMC_NORSRAMInitStructure.FMC_WriteOperation = FMC_WriteOperation_Enable; FMC_NORSRAMInitStructure.FMC_WaitSignal = FMC_WaitSignal_Disable; FMC_NORSRAMInitStructure.FMC_ExtendedMode = FMC_ExtendedMode_Disable; FMC_NORSRAMInitStructure.FMC_WriteBurst = FMC_WriteBurst_Disable; FMC_NORSRAMInitStructure.FMC_ContinousClock = FMC_CClock_SyncOnly; FMC_NORSRAMInitStructure.FMC_ReadWriteTimingStruct = &p; FMC_NORSRAMInitStructure.FMC_WriteTimingStruct = &p; FMC_NORSRAMInit(&FMC_NORSRAMInitStructure); /* Enable FSMC NOR/SRAM Bank1 */ FMC_NORSRAMCmd(FMC_Bank1_NORSRAM1, ENABLE); Any ideas what could be wrong? Kind Regards Jens #lcd-stm32f429-fmc2016-05-03 11:21 AM
Hello all,
my ST FAE solved the problem. I defined the Command and Data Address like this: #define LCD_BASE_Addr ((u32)(0x60000000|0x00000000)) #define LCD_BASE_Data ((u32)(0x60000000|0x00000001)) But because we have a 16Bit bus width I have to define the Data-Address with a offset of 2. #define LCD_BASE_Data ((u32)(0x60000000|0x00000002)) Now it works fine. Kind regards JensWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.