2017-02-17 11:47 PM
Hi
I am just a beginner in the STM32, I have been designing for 8bit Freescale parts for years. I am using ST's Nuleo64 STM32L07 processor.
Using STM32CubeMX I designed a very simple application that simply captures the system timer, GPIO interupt for the push button. I simply wrote some code (just for me getting used to the system) using Keil V5. I simply use the system timer interupt to blink the LED, pressing the button changes the speed of the LED . Within Cubemx I also selected RTC,LPUART but done nothing with the code yet. After building the application and ran it I noticed that the size of the code is 6420, and ram 1176. To me this seams a lot for what it does, I am used of having more tighter code. The application uses HAL library, does this put a large overhead to the size of code and ram used? And am I better stripping out some of the code that CubeMX creates?
Thanks
Scott
2017-02-24 12:21 PM
I guess Cortex M instruction set was designed to compete with 8 bit architecture. When code size is big, generate the MAP file to look into the details and which *.o file is bloated or which automatically linked ansi library file is attached.
Looking at the various teardowns (say from Ifixit) of popular consumer products should give some confidence level on the various flavours of the STM32 family:
STM32 M0 :
https://www.ifixit.com/Teardown/AirPods+Teardown/75578
STM32 M3 :
https://www.ifixit.com/Teardown/Apple+Pencil+Teardown/52955
STM32M4 :
2017-02-24 12:22 PM
STM32M4:
http://www.chipworks.com/about-chipworks/overview/blog/fitbit-alta-teardown
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.