2018-01-19 7:19 AM
I have been using Keil IDE for years (as a hobbyist).
Maybe someone who knows both Keil & TrueStudio could share some details about pros & cons.
I know that the primary difference is lack of licensing limits in TS (Keil - 32kB for non F0/L0 MCUs). I have Segger programmer/debugger (read that some features may need it on TrueStudio).
2018-05-15 7:31 AM
For educational purposes it would be nice if TS had a pure assembly project option, so that target MCU and debugger can be selected and then everything else is done by the user from scratch. This can easily be done in Keil.
2018-11-17 11:57 AM
Hello Andrew,
Would you mind please sharing what you mainly disliked in uVision? I see the most updated version is MDK 5.2.6. Have you ever tried it?
I am compelled to work Atollic now and after working with it for a month I can tell you that I hate it:
I am thinking to convince my boss to move to the MDK, so I am interested to know what are the features you're missing there?
2018-11-19 2:52 AM
I find the search, navigation, and browsing facilities particularly lame.
And some of the auto-format features were broken.
I haven't used it for a while now (been using Segger Embedded Studio lately), so I forget the precise details ...
ISTR that it kept applying the language auto-formatting inside comment?
"I see the most updated version is MDK 5.2.6"
You mean 5.26
"Have you ever tried it?"
No - still on 5.25. But I don't think the above features have significantly changed?
2018-11-19 3:51 AM
Hi Andrew,
I think I know you from LI - I always enjoy reading your comments. Thank you for spending your time to answer myself.
Actually I didn't claim 5.26 is better than 5.25, but just asked you. I personally had been using IAR for 10 years at least , until a few months ago. I think it also can be called lame, according to your definition. (-: I personally can get along with a relatively poor IDE ("lame"), since on my priority list, stability and debugger's quality and reliability have higher priority than GUI.
As for the Embedded Studio - it is interesting for me. I recently downloaded it and was impressed it is not as "hard" as Eclipse - i could open the application very quickly.
If you have one more minute for me, would you be so kind as to share some highlights of Embedded Studio pro's and con's, or maybe you could just answer these questions ?
Thank you once again!
2018-11-19 4:35 AM
Yes, the big plus of uVision is the debugging, which "just works" - unlike the nightmare of getting it to work in Eclipse.
And, of course, you get the ARM Compiler.
2018-11-19 4:38 AM
Thank you once again and good luck !
2020-07-13 10:05 AM
HI Guys, this might be a fairly old thread but just for anyone else who may still be interested in this. These are opinions on the two.
Pros of Keil
Pros of Truestudio
There are obviously a lot more differences between the two but I find that they are minor issues and probably don't need to be mentioned.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.