2020-06-18 11:10 AM
seems like the chances of a JVM on an MCU is a nightmare?
research show java is supposed to be cross platform, however it makes sense to be able to embed the virtual machine without difficulty first.
I can’t even find a successful case online except by an almost huge mini company
skygge
2020-06-18 11:43 AM
2020-06-18 1:41 PM
Java has a significant overhead requirement. Not something you can easily put into a microprocessor with limited RAM and FLASH available. If you can't find anything, there's probably a reason.
2020-06-18 2:16 PM
Can't imagine writing microcontroller code without pointers. Java exists, at least in part, because it is intended to be machine independent, hardly a typical microcontroller application. HAL was an attempt at creating a machine independent layer, but most of the code is crap and it turns out to be easier and quicker to write your own.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.