2021-04-24 9:02 AM
Hi all
i am facing a very strange issue on the MCU i have specified on the title. I am working on these devices since long time ago and i never had any kind of problem with them. During these days, i am experiencing a very strange issue: i can't connect to the microcontroller with my ST-LINK under IAR. I am able instead to connect with it through ST LINk and ST LINK Utility. I have noticed that the IWDG option bit is set to 0 ( unchecked). This means that the IWDG is runnig in hadware mode, and it could be provoking the issue with IAR, i hence tried to set it, but it remains unchecked.
Did anyone else experience the same? How can i solve it?
Thanks to all for helping me! I am really struggling with it!
Bye
CN
2021-04-25 10:43 PM
I can also add that i can't connect in Debug on these devices. It sounds very strange
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.