2021-06-23 10:07 AM
Hi!
I'm was writing C-code for the VL6180X because I find ST's own C-code library quite messy and I could not use it because I did not understand it. So I re-wrote a C++ library to STM32 C-code from https://github.com/pololu/vl6180x-arduino
Here is the code. (It's working now!)
https://github.com/DanielMartensson/STM32-Libraries/tree/master/VL6180X
Anyway! When I first tried to connect the I2C with the distance sensor.
#define VL6180X_ADDRESS_DEFAULT 0x29
HAL_StatusTypeDef status = HAL_I2C_IsDeviceReady(&hi2c1, VL6180X_ADDRESS_DEFAULT, 10, 100);I get status = HAL_ERROR
That's weard because I can use the VL6180X sensor from ST's own .hex file and it works great. But when I trying to compile own C-code, then it won't work.
It's nothing wrong at the Nucleo F401RE board nor the sensor. I have tried to connect a SSD1306 I2C LCD to the I2C as well, but then i get status = HAL_BUSY
This Nucleo Board came with the VL6180X Expension Board X-NUCLEO-6180XA1
Can it be some issues with the firmare?
static void MX_I2C1_Init(void)
{
/* USER CODE BEGIN I2C1_Init 0 */
/* USER CODE END I2C1_Init 0 */
/* USER CODE BEGIN I2C1_Init 1 */
/* USER CODE END I2C1_Init 1 */
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 100000;
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2C1_Init 2 */
/* USER CODE END I2C1_Init 2 */
}
Solved! Go to Solution.
2021-06-23 11:10 AM
HAL_I2C_IsDeviceReady returns HAL_ERROR if the device does not respond.
Slave addresses should be left-aligned. So use 0x52 instead (0x29 << 1).
2021-06-23 11:10 AM
HAL_I2C_IsDeviceReady returns HAL_ERROR if the device does not respond.
Slave addresses should be left-aligned. So use 0x52 instead (0x29 << 1).
2021-06-23 11:31 AM
Thanks. It's connected now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.