2021-05-05 5:54 AM
Hello,
On a pcb on which there is the STM32F030K6T6, I am facing a strange issue.
First, the context is that I am using different timers, interruptions, DMA, UART, analog inputs and digital outputs (PWM, ON/OFF signals).
2 of the i/o's are concerned by the issue:
When I am configuring the PA0 as input, with no pulling, the PB3 output can't be drive and remain low even if I order to go to high level. Other functionnalities seem to work fine, the only issue is the PB3 output and this thing happens to only 2 of my 8 prototypes ! The 6 others works fine even with this configuration.
When I am configuring the PA0 as output, push-pull type, it all works perfectly, even for the 2 which weren't working.
That thing doesn't make sense to me at all !
Is there something I am missing with the PA0 configuration as input ? maybe related to other peripherals configuration, i/o drive, etc as something as I souldn't configure it this way because I am already using something, somewhere ?
Thank you in advance,
2021-05-06 8:34 AM
In the problematic state, read out and check/post content of relevant GPIO registers.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.