2019-12-14 11:42 AM
STM32H7 should be pin compatible version of STM32F777 and STM32F479 with BGA216.
Or there should be an H4 running @ 400 Mhz.
2019-12-14 9:36 PM
This makes no sense, they have a different set of peripherals.
2019-12-15 7:49 AM
stm32f777 AND F469/79 ARE PIN TO PIN COMPATIBLE, H7 has only MDMA peripheral.
It has the jpeg engine, everything, double precision, etc.
There should an H4 then BGA216.
Leaving the best package out and claiming to be pin compatible.
Who would ever choose a 176 BGA with .65mm garbage routing over 240 .8mm easy routing.
ROFL? Hello...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.