2025-07-16 12:06 AM
Hello, ST experts
STM32F407 is used on our system. PE7 is configured as an EXTI pin for both rising and falling edge. How can I accurately recognize which edge is the cause of this interrupt? Because there maybe a narrow glitch on PE7, so reading GPIO state on interrupt routine may not be a good way.
Best Regards
Yang
Solved! Go to Solution.
2025-07-16 1:20 AM
If it's really important to catch a glitch, maybe have two EXTIs - one rising, and one falling?
@Yang Yang wrote:Rising edge means pre-shutdown, falling edge means shutdown(at least 3 seconds interval).
In this case, you know that the rising edge has to happen first - so set EXTI just for that.
Once that rising edge has occurred, then start your timing for the 3-second interval...
basically a debounce operation...
2025-07-16 12:57 AM
@Yang Yang wrote:Because there maybe a narrow glitch on PE7, so reading GPIO state on interrupt routine may not be a good way.
In that case, why does it matter which edge actually caused the interrupt?
Anyhow, it would have been the first edge - surely?
2025-07-16 1:09 AM
Hello,Andrew
Yes,it does matter which edge caused the interrupt. Different edges means different operations. Rising edge means pre-shutdown, falling edge means shutdown(at least 3 seconds interval).
By the way, think about this situation. Rising edge interrupt happened at 0 nano-second, but PE7 only keeps about 50 nano second, that means it goes low at 50 nano-seconds later. And interrupt routine clear the interrupt at about 1000 nano seconds later, is the falling edge interrupt ignored?
BR
Yang
2025-07-16 1:11 AM
Usually by checking the line status in the interrupt routine.
In case of a glitch, as Andrew Neil suggested, you are most probably too late anyway.
And the timing is unpredictable.
If this is a problem for your application, add a glitch filter.
This is usually a RC lowpass with a Schmitt trigger
2025-07-16 1:20 AM
If it's really important to catch a glitch, maybe have two EXTIs - one rising, and one falling?
@Yang Yang wrote:Rising edge means pre-shutdown, falling edge means shutdown(at least 3 seconds interval).
In this case, you know that the rising edge has to happen first - so set EXTI just for that.
Once that rising edge has occurred, then start your timing for the 3-second interval...
basically a debounce operation...
2025-07-16 1:26 AM
Hello, Ozone
I am very apprecaited for your help. I will have a try about your suggestion. And as I said, the falling edge will be ignored at that situation?(falling edge happened after interrupt routine clears pending register)
BR
Yang
2025-07-16 4:16 AM
I don't know your exact use case.
But you need to take system behavior in all plausible scenarios into account.
What happens if the second transition of a glitch happens before you even enter the interrupt (12 clk-cycle latency), or during the interrupt ?
Are those glitches of any relevance for your application, except of being an "annoyance" ?
As an example, all commercial ECUs we use have fixed or configurable glitch filters on DINs, defaulting to a 3dB frequency of a few kHz. Since our applications are based on a 10ms processing cycle, faster transitions/reactions are neither possible nor desired.
Other interfaces (like PWM or rotary encoders) are handled by specific peripherals, not software directly.
We have some self-designed legacy hardware designed in-house, which cause nothing but trouble in this regard.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.