2020-01-20 8:11 AM
I'm currently in the process of compiling example code from our supplier for an e-ink display. The issue however is it uses functions that predate HAL from what I can tell. While some things are simply renaming to uppercase, some other things are unknown.
Some examples are:
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB|RCC_APB2Periph_GPIOD|RCC_APB2Periph_GPIOE, ENABLE);
//SCL--PE0 SDA--PE1
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_Init(GPIOE, &GPIO_InitStructure);
GPIO_ResetBits(GPIOB, GPIO_Pin_8)
GPIO_SetBits(GPIOB, GPIO_Pin_8I'm currently using STM32CubeIDE
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.