2009-03-05 2:01 PM
Is there a problem with the FIFO of the SDIO?
2011-05-17 4:05 AM
Hello,
Could somebody confirm or explain where I am wrong with the following problem on a STM32F103ZET6 ? 1 – Can we only write once to the FIFO of the SDIO when DPSM is enabled? And Does the DPSM have to be enabled to write to the FIFO? 2 – Does this problem explain why we can only transfer data with 1 byte block (see errata section 2.13 Limited multibyte support with SDIO cards) /* SDIO configuration */ SDIO_InitStructure.SDIO_ClockDiv = (UI8)0x01; SDIO_InitStructure.SDIO_ClockEdge = SDIO_ClockEdge_Rising; SDIO_InitStructure.SDIO_ClockBypass = SDIO_ClockBypass_Disable; SDIO_InitStructure.SDIO_ClockPowerSave = SDIO_ClockPowerSave_Disable; SDIO_InitStructure.SDIO_BusWide = SDIO_BusWide_4b; SDIO_InitStructure.SDIO_HardwareFlowControl = SDIO_HardwareFlowControl_Disable; SDIO_Init(&SDIO_InitStructure); /* “FIFO� configuration with DPSM disabled */ SDIO_DataInitStructure.SDIO_DataTimeOut = SD_DATATIMEOUT; SDIO_DataInitStructure.SDIO_DataLength = 32; SDIO_DataInitStructure.SDIO_DataBlockSize = SDIO_DataBlockSize_32b; SDIO_DataInitStructure.SDIO_TransferDir = SDIO_TransferDir_ToCard; SDIO_DataInitStructure.SDIO_TransferMode = SDIO_TransferMode_Block; SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Disable; SDIO_DataConfig(&SDIO_DataInitStructure); /* try to write data in the FIFO */ SDIO_WriteData(0x00000001); SDIO_WriteData(0x00000002); SDIO_WriteData(0x00000003); SDIO_WriteData(0x00000004); /* RESULT */ /* reading the memory from 0x40018080 to 0x400180FC (FIFO address) everything is at 0, nothing is written */ /* other “FIFO� configuration with DPSM enabled */ SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Enable; SDIO_DataConfig(&SDIO_DataInitStructure); /* try to write data in the FIFO */ SDIO_WriteData(0x00000005); /* RESULT */ /* reading the memory from 0x40018080 to 0x400180FC (FIFO address). The full FIFO is written with 0x00000005 */ /* try to write again in the FIFO */ SDIO_WriteData(0x00000006); /* RESULT */ /* reading the memory from 0x40018080 to 0x400180FC (FIFO address). The full FIFO is STILL written with 0x00000005 */ /* reinit DPSM */ SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Enable; SDIO_DataConfig(&SDIO_DataInitStructure); /* try to write data in the FIFO */ SDIO_WriteData(0x00000007); /* RESULT */ /* reading the memory from 0x40018080 to 0x400180FC (FIFO address). The full FIFO is written with 0x00000007 */ /* try now to access the FIFO with pointer at different address */ UI32 *ptFifo; ptFifo = (UI32)0x40018084; /* reinit DPSM */ SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Enable; SDIO_DataConfig(&SDIO_DataInitStructure); /* try to write data in the FIFO */ *ptFifo = 0x00000008; /* RESULT */ /* reading the memory from 0x40018080 to 0x400180FC (FIFO address). The full FIFO is written with 0x00000008 */ INFO: seeing the behaviour of the FIFO, I didn’t check any registers such as SDIO FIFO Counter. Because DPSM is enabled, as soon as I write to the FIFO, data are transferred. Thanks in advance.2011-05-17 4:05 AM
I am also facing the same problem with FIFO in SDIO.
is it a known issue in STM32F103 series. What is the work around?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.