2017-07-13 3:49 AM
Dear sirs,
I want to make drive recorder.
I think to use, USB(Mass drive), SD card small, TFT window ,camera(I want many cameras).
I do not want to make a proper product. I want only education or hobby.
I found two products.
1,STM32F4x7
2,STM32F469VIT6
1 is get pic slowly? (I need to 15fps or over)
2 is employ both camera and TFT?
(I saw two function covered with a data sheet)
In addition, as for 2, are a camera and the LCD interface omitted with 100 pins and 144 pins?
thanks
#stm322017-08-07 1:12 AM
Dear
pa_papa_wolf
,You can use STM32 for USB Mass storage, camera and LCD at the same time.
To give you more info, we need more info about your request such as LCD resolution, camera resolution.
Best regards,
Tilen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.