2012-10-02 12:46 PM
Hello,
Everything is in the title, is it possible to use a DMA to transmit data on SWO ? Or at least to send data (multiple bytes) without blocking execution ? Thomas. #itm-dma-jtag2012-10-03 7:00 AM
You can always do a memory to memory DMA, but you would have to come up with some way to ensure the ITM queue has space for the DMA transfer. Given the relatively high data rate of ITM (I get 2Mbit/sec with an STM32F205 at 120MHz using J-Link SWO Viewer) it might be safe to use a timer to trigger a DMA transfer.
Jack Peacock2012-10-03 7:09 AM
It would depend if the core registers have in-bound access via the AHB, somehow I imagine they'd be like TCM/CCM and be unavailable to DMA.
As Jack suggest pace it with a timer, it'll either work or not, but I wouldn't spend a lot of time fighting with it.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.