2025-01-27 12:55 PM
Howdy,
I am working with the STM32U575 and wanting to use the lower power capabilities of the ADF. The problem is that, for me to get the use I am looking for out of the ADF, I need to operate it constantly at 4 MHz. For this reason, I want to maintain the HSE when the system enters stop mode 2. I know that this is not directly supported, but I was wondering if there is a way to do this anyway. I was also thinking that it could be possible to disable all the peripherals manually in a similar way as stop mode 2 and put the system in sleep mode. My one hesitation for this method is that I would need to dedicate so much time to finding every peripheral's interrupt register and disabling them. Any suggestions on how I should handle this would be much appreciated. Hope you all have a wonderful day. :)
Solved! Go to Solution.
2025-01-27 1:18 PM
Did you consider MSIK?
2025-01-27 1:18 PM
Did you consider MSIK?
2025-01-27 1:29 PM
Hi Uwe,
this is exactly what I was looking for. Thank you so much.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.