2021-08-04 3:48 AM
While testing the data line, I have connected a wire to an A0 pin which gives 25v on full throttle signal. After dumping the code can't get any output as expected and found few registers were heating up.
2021-08-04 4:11 AM
> Is it okay to connect a 25v wire on an A0 pin to The STM32F072RB Dev board?
No.
JW
2021-08-04 6:48 AM
The Absolute Maximum Values for pins are listed in the datasheet. In most cases, 5V is the max. In some cases, 3.3V (or operating voltage) is the max.
2021-08-04 8:52 AM
An 5 V on 5-Volt tolerant pins is also only allowed on a powered device!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.