2008-11-09 1:45 PM
Is I2S in STM32F103xC bidirectional?
2011-05-17 3:51 AM
Most of the I2Ss configuration are supported for output functions only.We know that STM32F103xC support 2 I2Ss in it's design. Are the I2Ss birectional? Or any STM microcontroller supports birectional I2S interface?
Thanks.2011-05-17 3:51 AM
Hi,
STM32 I2S features are : � Simplex communication (only transmitter or receiver) � Master or slave operations � 8-bit programmable linear prescaler to reach accurate audio sample frequencies (from 8 kHz to 48 kHz) � Data format may be 16-bit, 24-bit or 32-bit � Packet frame is fixed to 16-bit (16-bit data frame) or 32-bit (16-bit, 24-bit, 32-bit data frame) by audio channel � Programmable clock polarity (steady state) � Underrun flag in slave transmission mode and Overrun flag in reception mode (master and slave) � 16-bit register for transmission and reception with one data register for both channel sides � Supported I2S protocols: – I2S Phillips standard – MSB-Justified standard (Left-Justified) – LSB-Justified standard (Right-Justified) – PCM standard (with short and long frame synchronization on 16-bit channel frame or 16-bit data frame extended to 32-bit channel frame) � Data direction is always MSB first � DMA capability for transmission and reception (16-bit wide) � Master clock may be output to drive an external audio component. Ratio is fixed at 256 × FS (where FS is the audio sampling frequency) For More details refer to RM0008 (Reference Manual ) available on web Section : ''I2S functional description''. Cheers, ST1.2011-05-17 3:51 AM
Hi, STM1,
So from RM0008, the I2S in the high-density devices can be configured as audio in /audio out, right? So we can use the I2S to input digital audio to the high-density devices and output to host via some transport protocol like USB, is it correct? Thanks, Albert Hsu. :)2011-05-17 3:51 AM
I have hardware already implemented design that I must make work:
STM32F103ZG can I connect a single CODEC to both I2S2 in master TX, and I2S3 in slave RX? Will this work? Can it be made to work? If not I have to have 2 codecs, one connected to I2S2 in master TX, and the other to I2S3 in master RX right?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.