2020-05-29 9:35 PM
I have currently configured the SPI in the following configuration
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_16BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_HARD_OUTPUT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_ENABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 10;
my DMA settings are as follows
hdma_spi1_tx.Instance = DMA2_Stream3;
hdma_spi1_tx.Init.Channel = DMA_CHANNEL_3;
hdma_spi1_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_spi1_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi1_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi1_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_spi1_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi1_tx.Init.Mode = DMA_NORMAL;
hdma_spi1_tx.Init.Priority = DMA_PRIORITY_LOW;
hdma_spi1_tx.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
hdma_spi1_tx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_1QUARTERFULL;
hdma_spi1_tx.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_spi1_tx.Init.PeriphBurst = DMA_PBURST_SINGLE;
/* SPI1_RX Init */
hdma_spi1_rx.Instance = DMA2_Stream0;
hdma_spi1_rx.Init.Channel = DMA_CHANNEL_3;
hdma_spi1_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_spi1_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi1_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi1_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_spi1_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi1_rx.Init.Mode = DMA_NORMAL;
hdma_spi1_rx.Init.Priority = DMA_PRIORITY_LOW;
hdma_spi1_rx.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
hdma_spi1_rx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_1QUARTERFULL;
hdma_spi1_rx.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_spi1_rx.Init.PeriphBurst = DMA_PBURST_SINGLE;
There is a vague indication using timing diagram that NSS pulse output will be controlled by the SPI driver in TI Master mode
[Figure 252 pg no 884 .Reference manual
STM32F405/415, STM32F407/417, STM32F427/437 and
STM32F429/439 advanced Arm®-based 32-bit MCUs]
My SPI peripheral needs a NSS high pulse for Indicating end of frame.
Is there anything i should look into to enable NSS pulse mode so that i can use a DMA where the SPI driver triggers a NSS Pulse by itself between each frames
2020-05-29 10:15 PM
No, "NSS pulse" is available only in newer STM32 models.
As a workaround, you can use a timer to generate the NSS pulse, and use that time to trigger DMA instead of SPI Tx to load the SPI_DR.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.