2018-03-07 4:57 AM
My hardware is STM32F429ZI6 and LCD.
External ram or etc no other hardware.Is fsmc and fmc different?Is that valid this data for the command stm32f429?
#define LCD_REG (*((volatile unsigned short *) 0x60000000))
#define LCD_RAM (*((volatile unsigned short *) 0x60020000))These codes.
Stm32f407 also works.Why does stm32f429 not work? I see the reset and set on the lcd screen. Then there is the white screen.Thanks.
FSMC_NORSRAMInitTypeDef FSMC_NORSRAMInitStructure;
FSMC_NORSRAMTimingInitTypeDef FSMC_NORSRAMTimingInitStructure;FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM1;
FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable; FSMC_NORSRAMInitStructure.FSMC_MemoryType = FSMC_MemoryType_SRAM; FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_16b; FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable; FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low; FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable; FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState; FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable; FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable; FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait = FSMC_AsynchronousWait_Disable; FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Disable; FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Enable; FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &FSMC_NORSRAMTimingInitStructure; FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure); FSMC_NORSRAMTimingInitStructure.FSMC_AddressSetupTime = 1; //15 FSMC_NORSRAMTimingInitStructure.FSMC_AddressHoldTime = 1; //15 FSMC_NORSRAMTimingInitStructure.FSMC_DataSetupTime = 3; //255 FSMC_NORSRAMTimingInitStructure.FSMC_BusTurnAroundDuration = 0; //15 FSMC_NORSRAMTimingInitStructure.FSMC_CLKDivision = 1; //15 FSMC_NORSRAMTimingInitStructure.FSMC_DataLatency = 0; FSMC_NORSRAMTimingInitStructure.FSMC_AccessMode = FSMC_AccessMode_A; FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &FSMC_NORSRAMTimingInitStructure; FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure); FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM1, ENABLE);2018-10-01 3:09 AM
hi did you get solution(ili9341 8 bit parallel)..?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.