2018-01-09 6:39 PM
Hello,
I have couple of questions,
1. I would like to know, if I can use X-CUBE-MEMSMIC1 package with Digital MEMS Mic that I have instead of using X-NUCLEO-CCA02M1 MEMS Evaluation board. If so, how can I do it?
2. Can I modify the X-CUBE-MEMSMIC1 package projects (particularly AcousticBF) to work on STM32L471.
According to documentation, I should be able to modify the project source code to run on STM32L471. But I would like to if anyone else has tried doing soomething similar.
Regards.
2018-01-09 10:57 PM
Topic touched several times on this forum - I mean different boards but problem is the same.The CubeMX does not allow to automatically integrate BSP packages (drivers for nucleo modules, or other stuff on the discovery boards) with cube generated projects. So you have to manually modify delivered examples (needs some experience) OR generate the project automatically using CubeMX for resources required by particular board.
See my posts:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.