2021-06-18 12:03 PM
I am trying to measure the frequency of a square wave using TIM1 in direct input capture mode (STM32F3-DISCOVERY) . I can measure the frequency successfully , but i want to add an input prescaler, no matter what the value of prescalar i set i get the same value on my capture/compare register (CCR1).
My code for TIM1:
void TIM1_IC_INIT(void) {
RCC->AHBENR |= RCC_AHBENR_GPIOAEN; //ENABLE GPIOA CLOCK
RCC->APB2ENR |= RCC_APB2ENR_TIM1EN; //ENABLE TIMER CLOCK
RCC->CFGR3 |= RCC_CFGR3_TIM1SW; //SELECT CLOCK SOURCE PLLCLK*2
GPIOA->MODER |= GPIO_MODER_MODER8_1; //SET GPIO TO ALETERNATE FUNCTION
GPIOA->AFR[1] |= 6 << GPIO_AFRH_AFRH0_Pos; //AF6 FOR PA8 , TIM1_CH1
TIM1->SMCR |= 5 << TIM_SMCR_TS_Pos | TIM_SMCR_SMS_2; //RESET MODE
TIM1->CCMR1 |= 1 << TIM_CCMR1_CC1S_Pos; //CONFIGURE CH1 AS INPUT
TIM1->CCER &= ~(TIM_CCER_CC1P | TIM_CCER_CC1NP); //RISING EDGE POLARITY
TIM1->CCMR1 |= 3 << TIM_CCMR1_IC1PSC_Pos; //SET A PRESCALER OF 8
TIM1->CCER |= TIM_CCER_CC1E; //ENABLE CAPTURE
TIM1->CR1 |= TIM_CR1_CEN; // START TIMER
}While debugging I checked the value of CCMR1 to check if the prescaler bits have been set properly and yes they were, Value of IC1PSC[3:2] is set to 0b11. I dont know where the problem is, any ideas?
Solved! Go to Solution.
2021-06-18 12:26 PM
The input to slave-mode controller is not prescaled, i.e. each rising edge will reset the counter, so the captured value is from the previous reset i.e. previous edge, no matter what is the prescaler.
Don't use the slave-mode controller reset, rather, calculate the frequency from difference of two consecutive captured values.
JW
2021-06-18 12:26 PM
The input to slave-mode controller is not prescaled, i.e. each rising edge will reset the counter, so the captured value is from the previous reset i.e. previous edge, no matter what is the prescaler.
Don't use the slave-mode controller reset, rather, calculate the frequency from difference of two consecutive captured values.
JW
2021-06-18 1:35 PM
thank you so much, that solves it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.