2018-01-24 12:44 AM
I'm using an STM32F401RET with code generated in the cube(v4.23) with F4 library(v1.18).
The ADC is set up to sample one channel under a trigger from a timer with the values going to DMA. When 256 samples have been collected the conversion complete call back is called and I copy the data off and start an injected sequence consisting of CH15, Vref and Temp ADC channels.
When I do this only the first injected channel data register has data in it. I have gone through the config register values and they all look correct.
Also if I manually change the ADC_JSQR->JL value then the captured adc value changes, and follows the order of the ranked values. I.e. Len=3 result=rank1_ADC,
Len=2 result=rank2_ADC, Len=1 result=rank3_ADC.
User code below(removed data storing):
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{ HAL_ADC_Stop_DMA(&hadc1);HAL_ADCEx_InjectedStart(hadc);HAL_ADCEx_InjectedPollForConversion(hadc,8);HAL_ADC_Start_DMA(&hadc1, (uint32_t *)acBatteryDataDMA, ADC_AC_DATA_LEN);}Config Code below:
void MX_ADC1_Init(void)
{ ADC_ChannelConfTypeDef sConfig; ADC_InjectionConfTypeDef sConfigInjected;/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/ hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4; hadc1.Init.Resolution = ADC_RESOLUTION_12B; hadc1.Init.ScanConvMode = DISABLE; hadc1.Init.ContinuousConvMode = DISABLE; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING; hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T2_TRGO; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.NbrOfConversion = 1; hadc1.Init.DMAContinuousRequests = DISABLE; hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV; if (HAL_ADC_Init(&hadc1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/ sConfig.Channel = ADC_CHANNEL_14; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_112CYCLES; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Configures for the selected ADC injected channel its corresponding rank in the sequencer and its sample time
*/ sConfigInjected.InjectedChannel = ADC_CHANNEL_15; sConfigInjected.InjectedRank = 1; sConfigInjected.InjectedNbrOfConversion = 3; sConfigInjected.InjectedSamplingTime = ADC_SAMPLETIME_112CYCLES; sConfigInjected.ExternalTrigInjecConvEdge = ADC_EXTERNALTRIGINJECCONVEDGE_NONE; sConfigInjected.ExternalTrigInjecConv = ADC_INJECTED_SOFTWARE_START; sConfigInjected.AutoInjectedConv = DISABLE; sConfigInjected.InjectedDiscontinuousConvMode = DISABLE; sConfigInjected.InjectedOffset = 0; if (HAL_ADCEx_InjectedConfigChannel(&hadc1, &sConfigInjected) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Configures for the selected ADC injected channel its corresponding rank in the sequencer and its sample time
*/ sConfigInjected.InjectedChannel = ADC_CHANNEL_VREFINT; //sConfigInjected.InjectedChannel = ADC_CHANNEL_14; sConfigInjected.InjectedRank = 2; if (HAL_ADCEx_InjectedConfigChannel(&hadc1, &sConfigInjected) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Configures for the selected ADC injected channel its corresponding rank in the sequencer and its sample time
*/ sConfigInjected.InjectedChannel = ADC_CHANNEL_TEMPSENSOR; sConfigInjected.InjectedRank = 3; if (HAL_ADCEx_InjectedConfigChannel(&hadc1, &sConfigInjected) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.