2020-08-06 12:47 AM
i used SDIO project to read micosd card in STM32 Standard Peripheral Libraries
when i upload code and debug
__IO SD_Error errorstatus = SD_OK;
uint32_t response = 0, count = 0, validvoltage = 0;
uint32_t SDType = SD_STD_CAPACITY;
/*!< Power ON Sequence -----------------------------------------------------*/
/*!< Configure the SDIO peripheral */
/*!< SDIO_CK = SDIOCLK / (SDIO_INIT_CLK_DIV + 2) */
/*!< on STM32L1xx devices, SDIOCLK is fixed to 48MHz */
/*!< SDIO_CK for initialization should not exceed 400 KHz */
SDIO_InitStructure.SDIO_ClockDiv = SDIO_INIT_CLK_DIV;
SDIO_InitStructure.SDIO_ClockEdge = SDIO_ClockEdge_Rising;
SDIO_InitStructure.SDIO_ClockBypass = SDIO_ClockBypass_Disable;
SDIO_InitStructure.SDIO_ClockPowerSave = SDIO_ClockPowerSave_Disable;
SDIO_InitStructure.SDIO_BusWide = SDIO_BusWide_1b;
SDIO_InitStructure.SDIO_HardwareFlowControl = SDIO_HardwareFlowControl_Disable;
SDIO_Init(&SDIO_InitStructure);
/*!< Set Power State to ON */
SDIO_SetPowerState(SDIO_PowerState_ON);
/*!< Enable SDIO Clock */
SDIO_ClockCmd(ENABLE);
/*!< CMD0: GO_IDLE_STATE ---------------------------------------------------*/
/*!< No CMD response required */
SDIO_CmdInitStructure.SDIO_Argument = 0x0;
SDIO_CmdInitStructure.SDIO_CmdIndex = SD_CMD_GO_IDLE_STATE;
SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_No;
SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No;
SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable;
SDIO_SendCommand(&SDIO_CmdInitStructure);
--------------------
Error here SDIO_Init(&SDIO_InitStructure);
crash when debug SDIO_Init(&SDIO_InitStructure);
Please help me
2020-08-06 3:11 AM
What does "crash" mean here? If it hard faults, examine the SCB registers to find out why.
2020-08-10 3:36 AM
may be pin mismatch issue .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.